2022-01-12 5:48 AM
Hi Guys,
I'm writting a bootlader/application for STM32L4 in STM32CubeIDE i I want my app to run even if there is no bootloader in memory.
This is my *.ld file:
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x20000000, LENGTH = 96K
RAM2 (xrw) : ORIGIN = 0x10000000, LENGTH = 32K
FLASH (rx) : ORIGIN = 0x8001000, LENGTH = 1024K-0x1000
BOOT (rx) : ORIGIN = 0x8000000, LENGTH = 131K
}I my app source I have the below function (which is properly placed at 0x8000000 in flash) :
#define MY_BL_FUNCTIONS __attribute__((section(".bootsection")))
void __attribute__((optimize("O0"))) Bootloader_JumpToApplication(void); MY_BL_FUNCTIONS
void __attribute__((optimize("O0"))) Bootloader_JumpToApplication(void)
{
asm("ldr R0,=0x8001004"); //my app start address
asm("BX R0"); //jump to app
}Unfortunately asm("BX R0") makes a sudden jump to my HardFault_Handler. instead of 0x8001004.
What do I do wrong?
Thanks in advance
Tom
2022-01-12 6:09 AM
Hello Tom,
Perhaps try "asm("ldr R0,=0x8001005"); //my app start address"
I believe Thumb-2 addresses are designated by bit-0 set.
Good Luck,
Dave
2022-01-12 6:29 AM
Show disasm.
> function (which is properly placed at 0x8000000 in flash)
A minimal vector table has to be at 0x0800'0000, with address of that function (possibly 0x0800'0009, if it follows immediately after that vector table) at 0x0800'0004.
[EDIT] Oh, and the displacement may be too far to use the pc-relative addressing (to which ldr R0, =xxxx translates)
https://developer.arm.com/documentation/dui0552/a/the-cortex-m3-instruction-set/memory-access-instructions/ldr--pc-relative
JW
2022-01-12 6:31 AM
No, doesn't work like that.
Also Vector Table, is a TABLE OF ADDRESSES, NOT CODE, Thumb code has an ODD address, the Cortex-M can't execute 32-bit ARM code, with EVEN addresses.
2022-01-12 6:43 AM
Thanks guys, I changed my bootloader func. to:
SCB->VTOR=0x8001000;
asm("ldr R0,=0x8001004");
asm("BX R0");tried asm("ldr R0,=0x8001005"); too but same result.
Of course I also did in system_stm32l4xx.c:
#define VECT_TAB_OFFSET 0x1000This is my disassembly:
08000000: push {r7}
08000002: add r7, sp, #0
08000004: ldr r3, [pc, #16] ; (0x8000018 <Bootloader_JumpToApplication+24>)
08000006: ldr r2, [pc, #20] ; (0x800001c <Bootloader_JumpToApplication+28>)
08000008: str r2, [r3, #8]
0800000a: ldr r0, [pc, #20] ; (0x8000020)
0800000c: bx r0
0800000e: nop
08000010: mov sp, r7
08000012: ldr.w r7, [sp], #4
08000016: bx lr
08000018: stc 0, cr14, [r0, #-0]
0800001c: asrs r0, r0, #32
0800001e: lsrs r0, r0, #32
08000020: asrs r4, r0, #32
08000022: lsrs r0, r0, #32
08000024: ; <UNDEFINED> instruction: 0xffffffff
08000028: ; <UNDEFINED> instruction: 0xffffffff
0800002c: ; <UNDEFINED> instruction: 0xffffffff
08000030: ; <UNDEFINED> instruction: 0xffffffff
08000034: ; <UNDEFINED> instruction: 0xffffffffTom
2022-01-12 6:49 AM
LDR Rx,= will translate to an ADD/SUB (near or further) with PC for short compatible addresses, an immediate move if the constant packs, or a PC relative load access to a literal pool.
What you can't do is branches to the entire 32-bit address space
2022-01-12 6:52 AM
VECTOR TABLE != CODE
What are words at 0x08000000 and 0x08001000 should be initial SP/PC pair at minimum
Execution starts assuming SCB->VTOR = 0, memory mapped at zero depends on BOOT pins, and can be ROM, FLASH or RAM
ldr r0,=0x08001004
ldr r0,[r0, #0] ; Load ADDRESS in VTOR+4
bx r0
2022-01-12 3:39 PM
Apart from the official documentation by ARM and ST, the internet is full of materials about Cortex-M vector table, startup scripts etc.
FLASH (rx) : ORIGIN = 0x8001000, LENGTH = 1024K-0x1000
BOOT (rx) : ORIGIN = 0x8000000, LENGTH = 131K0x1000 = 4K. Those regions have an overlap of a 127K!
> I want my app to run even if there is no bootloader in memory.
You are misunderstanding what a bootloader is. Bootloader is a code that is always present and always capable of recovering a device to a fully working condition. If there is some boot/update code that can be missing or otherwise broken at some point, then that is a second (stage) bootloader.
2022-01-13 12:59 AM
Hi Piranha
The overlap is no the problem here, as everything goes into flash as expected as you could see.
I understand how bootloader works but at dev stage in order to flash bootloader and app I'd have to manuallly merge bootloader hex and app hex before programming which I dont want cause it makes no sense. It is easier to place a simple jump at 0x8000000 to the app so I can quickly debug and run the app in CubeIDE.
2024-06-19 12:01 PM
Any solution?