Other tools (MCUs)

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Demo program for STM32F769I DISCO board is not compiling in SW4STM32 IDE. ERROR "recipe for target ‘Middlewares/USBH_Library/Core/usbh_core.o’ failed"

IHello,I am new to stm32 board, I have a new STM32F769I DISCO board.I have downloaded the firmware�?en.stm32cubef7_v1-16-0�? from ST.com to run a “STemWin�? project under “demonstration�? folder for “STM32F769I-Discovery�?.While Build project i get t...

PULAG.1 by Associate
  • 369 Views
  • 2 replies
  • 0 kudos

Resolved! Problem with step one opening example file?

Carefully following the instructions I got with my STM32 Nucleo board I am trying to opent the: C:\Users\myname\STM32Cube\Repository\STM32Cube _FW_L4_V1.11.0\Projects\NUCLEOL476RG\Examples_LL\ GPIO\GPIO_InfiniteLedTogglingThen project:GPIO_InfiniteLe...

0693W000001tTMAQA2.jpg
WBerr.2 by Associate
  • 392 Views
  • 3 replies
  • 0 kudos

Issues migrating from FP 1.3.2 to 1.4.0

Hello thereI started developing my custom boards (with H743 and H750) using Cube FP 1.3.0 and then 1.3.2. Now I have the new revision for both H7 so I've updated CubeMX to 5.2.1 and FP to 1.4.0 and now I've got a lot of troubles:1) USB MSC stoped wo...

Pedro3 by Senior
  • 129 Views
  • 1 replies
  • 0 kudos

Error on compiling of the buck-boost example of AN4449

Hello,I would like to use the example of AN4449 on SW4STM32.When building, I have 3 errors :fatal error: opening dependency file Drivers/BSP/STM32F3348-Discovery/stm32f3348_discovery.d: No such file or directorymake: *** [Drivers/BSP/STM32F3348-Disco...

vguil by Associate
  • 151 Views
  • 0 replies
  • 0 kudos