STM32 MCUs Motor control

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MCSDK 6.3.0 is out!

Dear MCSDK users, MCSDK version 6.3 is now available: Download It here. Here are the main changes for this version: Motor Control Features: FOCAdded C0 single shunt topology support.6StepThis algorithm has been enhanced on MCSDK version 6.3 release ...

GMA by ST Employee
  • 821 Views
  • 1 replies
  • 2 kudos

Resolved! Evspin32G4 - dual

Hello All,I just Bought an Evespin32G4 dual Board.https://www.st.com/en/evaluation-tools/evspin32g4-dual.html I completed the configuration using the X-CUBE-MCSDK-6.Goal: I will command 2 motors 36V, 4A (Moteur Hoverboard)I generated the cube ide pro...

ItzSam by Associate II
  • 814 Views
  • 8 replies
  • 2 kudos

Resolved! Bug in generated MC workbench code

Hello,I am using MC Workbench v. 6.2.1. The function "__weak bool MCI_StartWithPolarizationMotor(MCI_Handle_t* pHandle)" is supposed to return true on success. But it is currently returning false. This function is located in "mc_interface.c" at line ...

OleB by Associate
  • 367 Views
  • 2 replies
  • 1 kudos

Acim Gui

Hello;I haven't found the ACIMGUI under the files or Motor workbench. Can i take old version or recently versions links?