STM32 MCUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F401 USB CDC stuck in IRQ loop

Posted on February 18, 2015 at 10:27Hi,I'm using the USB Host library 2.1.0 (with USB_OTG_FS) on an STM32F401CD. Using the USB CDC code I'm having the following issue:When the STM32 is connected to a PC but no application on the PC has the port open...

gw by Associate II
  • 447 Views
  • 2 replies
  • 0 kudos

Low power USB host solution

Posted on March 30, 2013 at 12:43Hi all, I'm using STM32F100 processors for a while now and i had no issue so far. I'm looking for a solution that provides USB host functionality to a Flash disk but it must  be powered by battery, so it must by ener...

Labels