User Activity

Is there an official docker image for stm32cubeide - we are building our firmware in an azure devops pipeline, and downloading the latest stm32cubeide deb package and installing it is time-consuming for the build. Looking on docker hub there are a nu...
In CubeIDE 1.14, I can build a project in debug configuration (verified by output like 14:55:15 **** Incremental Build of configuration Debug for project ThermaWiFiII **** and file system changes).However, the build analyzer still continues to show m...
Hi,I'm migrating a headless build script we've used before to 1.14.0 - and it seems to fail with all the targets 2024-03-11T16:43:16.0230489Z /opt/st/stm32cubeide_1.14.0/stm32cubeide -data "/home/vsts/work/1/s/2023firmware/ws/" --launcher.suppressErr...
Is there an example for the x-cube-azrtos-l4 usbx stack showing how to implement the additional string descriptions and GET_OS_FEATURE_DESCRIPTOR features to allow an HID device to appear as WinUSB?
On an device running USBX/AzureRTOS, when I plug/unplug it from the computer - it doesn't always come back up device->ux_slave_device_state stays at UX_DEVICE_ATTACHED, and windows gives a Device Descriptor read failed (and a USB device not recognise...
Kudos from