User Activity

Posted on January 18, 2018 at 06:44I have a question regarding the WWDG in STM32F103RB. What can be the maximum timeout using the WWDG or even better question will be what will be the optimum value of the APB1 clock period(ms).I know the Maximum va...
Posted on January 17, 2018 at 06:12I am getting problem while making the &sharpIWDG work with the hardware watchdog feature in &sharpSTM32F103RB. I am doing this so that the watchdog is automatically enabled at power-on. To make the hardware option ...
Posted on January 04, 2018 at 08:21I am programming and debugging Nucleo STM32F103RB using external ST-LINKv2. To use the external ST-LINKv2 I have removed SB2 and SB12 from the Nucleo Board (Please see the Image for the function of specific SB). I ...