STM32 MCUs Boards and hardware tools

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Re-Generating with CubeMX sets the project to ST-LinkV2 instead of ST-LinkV3. It will not recover until I delete the generated folders. Initially CubeMX generates correctly.

I am working with IAR EWARM 9.10.1 and STM32CubeMX 6.2.1 on a NUCLEO-H743ZI2.To reproduce:Create NUCLEO-H743ZI2 project in STM32CubeMXGenerate itStart IARDownload to target (compile & flash succeed)Change something in IAR, e.g. add a source file to p...

FZida.1 by Associate
  • 451 Views
  • 2 replies
  • 0 kudos

Can the ST-LINKv3 interface on the DISCO board be used with IAR Workbench to run workbench in simultaneous dual-core debug mode ( master/slave project constructs )?

I have seen simultaneous or synchronous dual-core debugging within Workbench using the I-Jet from IAR, and I believe the DISCO board has an interface for connecting an I-Jet to; however, I'm wondering why the ST-LINKv3 can't do it, as it supports sha...