Resolved! Is it possible to flash the new version directly in STM32 ST-Link?
Hello,I flash my STM32 boards with the STM32 ST-Link Tool. But everytime I update my hex file I have to select the new one manually. Is there a way to let to do it itself?
Hello,I flash my STM32 boards with the STM32 ST-Link Tool. But everytime I update my hex file I have to select the new one manually. Is there a way to let to do it itself?
Posted on September 21, 2017 at 12:34Hi,I am trying to obtain real time variable reading in STM Studio But When My STM Board starts running program My STM Studio was unable to detect STLInk V2 and My program Runs only in Flash Mode.I am using ST Lin...
Posted on March 04, 2017 at 16:59Hi, I've developp a small product based on STM32L051, and we have to start production, 100 product for the moment.What is the best way to program STM32 after PCB mounting :- using STlink tool, connect each board and ...
Posted on December 01, 2017 at 16:13I can connect to my MCU with the ST-Link Utility and ST-Link V2. I can perform an erase of Bank 1 and Bank 2(Target -> Erase Bank1). I can perform an erase of all flash pages (Target -> Erase Sectors...). Howev...
Posted on October 10, 2017 at 18:26Hi,I am using a stm32f411 with 512Kbyte flash.I want to create a dump hex file of the flash as a backup.What is the Value of 'Size' 0x???? I have to write into the st link utility form to create an exact dump of 5...
Posted on August 04, 2017 at 21:43Hi,We have used J-LINK and J-Flash to program STM32F ARM families for a while and now planning to use ST-LINK and ST-LINK utility instead.We have merged bootloader and application code to make hex file for productio...
Posted on July 31, 2017 at 15:54Has anyone seen, or tried to use, a direct USB API to STM32 ST-LINK CLI v3.0.0.0 (the STLink on a STM32-NUCLEO board)? Ideally, for Windows 7 or newer?I have some manufacturing tests, which validate HW on an STM32L152...
Posted on May 19, 2017 at 17:25Hi!When I flash a .hex or .bin file with a ST-LINK V2 device on my STM32F4 microcontroller (with ST-LINK utility), the program only works if both the ST-LINK V2 and my MCU board stay connected to the computer (through ...
Posted on December 29, 2016 at 14:58Hello,I use ST-Link Utility v4.0.0 and STM32F103RC.CommandST-LINK_CLI.exe -c SWD -OB RDP=1gives message 'could not update the option bytes' but option bytes updated. And command returns an error code.GUI gives the...
Posted on February 24, 2016 at 08:27I have several discovery boards and last week I got a nucleo board. I made a mistake and connected another SWD debugger to STM32F103 SWD pins instead of on-board target microcontroller and erased ST-Link firmware....