STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DCMIPP silient failure

Hello team, Another day,  new same issue. :pensive_face:I have setup the DCMIPP PIPE 1 for the stm32n6570 DK, so that it dumps frames in address 0x34200000 which maps to SRAM3 begin address I have enabled bothe the memories SRAM3 and SRAM4 but with o...

KamurasiJordanArthur_2-1761801451579.png

Static DFU Serial Number on STM32F723xx

There have been previous posts about determining how the DFU serial number is formed from the 96-bit Unique ID.  However, when using the ROM bootloader for the STM32F723xx MCU I don't see unique serial numbers at all.  I am always seeing the same DFU...

jwj by Visitor
  • 38 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H743 USB CDC HardFault

Hi ST Community,    Our project uses STM32H743 (LQFP100). The system clock is set at the max 480MHz. The USB Device interrupts would occasionally cause a HardFault. For example, if we plug in or unplug the USB. The data hpcd would occasionally be 0xF...

Jerry_Hu_1-1761243064154.png Jerry_Hu_0-1761242223741.png
Jerry_Hu by Associate II
  • 240 Views
  • 5 replies
  • 0 kudos

Resolved! SPI4 RXNE never raises on STM32G4

Hello, my project is using all 4 SPI interfaces on the STM32G474. SPI1-3 all work flawlessly, but SPI4 never triggers the RXNE flag. All SPI buses are configured identically, with the only differences being the pinouts and APB1 vs 2 bus. I am polling...

amo25 by Visitor
  • 108 Views
  • 7 replies
  • 5 kudos