cancel
Showing results for 
Search instead for 
Did you mean: 

How to use the “Examples” project in STM32CubeF4 (LTDC_Display_2Layers)

chachamaru
Senior

 

Hello,

I am using STM32CubeIDE with the STM32F429I-Discovery board,
and my goal is to connect it with the MT9M001 camera module.
As a first step toward that, I would like to make the LCD display work properly.

In the STM32Cube_FW_F4_V1.28.0 package,
there are many sample projects organized as follows:

 

 
Projects > STM32F429I-Discovery > Examples > LTDC > LTDC_Display_2Layers

 

If I import this Example project into STM32CubeIDE,
will the LCD automatically display the sample image?
Or do I need to perform some additional setup or configuration steps?

I would appreciate any advice or guidance.

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @chachamaru 

According to the readme.txt file of the example.  After compiling and loading the project. It should display the image without need for any other configuration. 
PS: tested with the RevC of the Boards according to the same readme file.

Best Regards.

II

View solution in original post

3 REPLIES 3
Issamos
Lead III

Hello @chachamaru 

According to the readme.txt file of the example.  After compiling and loading the project. It should display the image without need for any other configuration. 
PS: tested with the RevC of the Boards according to the same readme file.

Best Regards.

II

MM..1
Chief III

Reply from @Issamos is true for some revesions DK, but for other not and still exist more as one REV board.

Thank you for your reply.


I was able to get the program running.