2025-11-03 11:38 AM
Hello, my project is using all 4 SPI interfaces on the STM32G474. SPI1-3 all work flawlessly, but SPI4 never triggers the RXNE flag. All SPI buses are configured identically, with the only differences being the pinouts and APB1 vs 2 bus. I am polling the transactions directly.
Initialization:
if (hspi_.Instance == SPI1)
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI1);
else if (hspi_.Instance == SPI2)
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI2);
else if (hspi_.Instance == SPI3)
LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_SPI3);
else if (hspi_.Instance == SPI4)
LL_APB2_GRP1_EnableClock(LL_APB2_GRP1_PERIPH_SPI4);
LL_SPI_SetMode(hspi_.Instance, LL_SPI_MODE_MASTER);
LL_SPI_SetTransferDirection(hspi_.Instance, LL_SPI_FULL_DUPLEX);
LL_SPI_SetDataWidth(hspi_.Instance, LL_SPI_DATAWIDTH_8BIT);
LL_SPI_SetClockPolarity(hspi_.Instance, LL_SPI_POLARITY_LOW);
LL_SPI_SetClockPhase(hspi_.Instance, LL_SPI_PHASE_1EDGE);
LL_SPI_SetBaudRatePrescaler(hspi_.Instance, LL_SPI_BAUDRATEPRESCALER_DIV256);
LL_SPI_SetTransferBitOrder(hspi_.Instance, LL_SPI_MSB_FIRST);
LL_SPI_SetStandard(hspi_.Instance, LL_SPI_PROTOCOL_MOTOROLA);
LL_SPI_SetNSSMode(hspi_.Instance, LL_SPI_NSS_SOFT);
SET_BIT(hspi_.Instance->CR1, SPI_CR1_SSI);
LL_SPI_SetRxFIFOThreshold(hspi_.Instance, LL_SPI_RX_FIFO_TH_QUARTER);
LL_SPI_DisableNSSPulseMgt(hspi_.Instance);
LL_SPI_DisableCRC(hspi_.Instance);
LL_SPI_Enable(hspi_.Instance);
Transfer:
void write(uint8_t* data, size_t len) {
for (uint16_t i = 0; i < len; i++)
{
while (!LL_SPI_IsActiveFlag_TXE(hspi_.Instance)) {}
LL_SPI_TransmitData8(hspi_.Instance, data[i]);
while (!LL_SPI_IsActiveFlag_RXNE(hspi_.Instance)) {}
(void)LL_SPI_ReceiveData8(hspi_.Instance);
}
while (LL_SPI_IsActiveFlag_BSY(hspi_.Instance)) {}
return;
}
For SPI1-3, write works fine. For SPI4, it hangs on the while RXNE wait forever.
I verified SPI4 is enabled (check RCC_APB2ENR) and not held in reset (check RCC_APB2RSTR):
# RCC_APB2ENR SPI4_EN
(gdb) p/x *0x40021060 >> 15 & 1
$25 = 0x1
# RCC_APB2RSTR SPI4_RST
(gdb) p/x *0x40021040 >> 15 & 1
$20 = 0x0I can reproduce this across multiple boards and eval boards. Any idea what is wrong?
Solved! Go to Solution.
2025-11-03 11:44 AM
If SCK line isn't toggled, RXNE won't get set. Verify the SCK line is actually active with a scope or logic analyzer. Barring that, verify the pin can be toggled freely when driven in output mode. Verify pins are set to VERY_HIGH frequency, or whatever is appropriate for the speed you are using.
2025-11-03 11:44 AM
If SCK line isn't toggled, RXNE won't get set. Verify the SCK line is actually active with a scope or logic analyzer. Barring that, verify the pin can be toggled freely when driven in output mode. Verify pins are set to VERY_HIGH frequency, or whatever is appropriate for the speed you are using.
2025-11-03 12:11 PM - edited 2025-11-03 12:13 PM
The pins are AF_PP, NOPULL, and VERY_HIGH speed. I can drive them manually in OUTPUT_PP with no issue.
SCK is active and toggling, but I notice it is at a way lower voltage level (1.5-2.5V) than expected, though this may be a problem with my board - would this cause issues or is the SCK->RXNE connection internal?
For what it's worth, I see RXNE fail to respond on the NUCLEO-G474RE eval board as well, which does not have PE2/5/6 exposed.
2025-11-03 12:15 PM
Is SSM bit set?
2025-11-03 12:19 PM
Yes, SSM is set.
(gdb) p hspi_.Instance
$1 = (SPI_TypeDef *) 0x40013c00
(gdb) p/x hspi_.Instance->CR1
$2 = 0x37c
(gdb) p/x hspi_.Instance->CR1 >> 9 & 1
$3 = 0x1
2025-11-03 12:20 PM
@amo25 wrote:SCK is active and toggling, but I notice it is at a way lower voltage level (1.5-2.5V) than expected,
If the level is too low, the STM32 will just see it as a constant low - ie, as no clock.
As already noted, if the STM32 sees no clock, nothing will be clocked-in and RXNE won't get set.
2025-11-03 12:43 PM
> The pins are AF_PP, NOPULL, and VERY_HIGH speed. I can drive them manually in OUTPUT_PP with no issue.
> SCK is active and toggling, but I notice it is at a way lower voltage level (1.5-2.5V) than expected,
Is SCK PE2? And if you toggle it "manually" as GPIO Output, is its amplitude correct, or lower too?
> would this cause issues or is the SCK->RXNE connection internal?
As others said, yes, this would cause issues, the Rx even in Master uses the input version of the SCK.
> For what it's worth, I see RXNE fail to respond on the NUCLEO-G474RE eval board as well, which does not have PE2/5/6 exposed.
That's irrelevant, there's no PE port on the 64-pin (and 48-pin) 'G474, thus "no" SPI4 - look at the peripherals list/table in the datasheet, for the 48/64-pin variant, there are only 3 SPIs.
JW
2025-11-03 12:58 PM
Thank you all for the input. The voltage sag was indeed the problem, depopulating the SPI4 bus brings the line back up to 3.3V and RXNE raises as expected.