STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! SDIO eMMC access failed in SDIO_CK without division

Hello all.I use STM32F4 controller with eMMC external Flash.I use two IDEs:IAR version 8.30STM32CubeIDE version 5.2.0The access to eMMC external Flash succeeds while I use IAR IDE.The access to eMMC external Flash failed while I use STMCubeIDE with ...

STM32CubeIDE THROWS EXCEPTION

above is the error that appears while I am creating a new project with STM32CubeIDEAny idea what's going on here?Has anybody actually gotten this stuff to work?Thanks,Best regards,Zhiming li

0693W00000D25YTQAZ.png
Zli.3 by Associate
  • 1008 Views
  • 1 replies
  • 0 kudos

Cube IDE installation under win7-64 SP1

This issue is all over the internet, and as usual with no good solutions.One of the two files which Cube says is not present actually is in that directory. I am totally stuck, having spent a day on this and downloading all sorts of VC++ redistributab...

0693W00000DpmthQAB.jpg 0693W00000DpmtSQAR.jpg 0693W00000DpnNwQAJ.jpg
PHolt.1 by Senior III
  • 5905 Views
  • 9 replies
  • 0 kudos

My STM32CubeIDE 1.5.0 crashing on startup.

Hello, I have a problem with STM32CubeIDE 1.5.0. After installation first run works just fine, second time I launch the problem it crashes on startup.I reinstalled multiple times and running of it ideas. There's an log file: https://pastebin.com/VtS4...

JZysk.1 by Associate II
  • 2655 Views
  • 4 replies
  • 0 kudos

CanFestival-3 for STM32H755 TPDO problem

hello everyone,I'm trying to import canfestival library in the STM32 project. I'm using STM32CubeIDE as IDE for my project. The library is imported correctly and 90% of functionality works well but I'm not able to set the timing for PDO. In attach y...

0693W00000DqBj8QAF.png 0693W00000DqBjNQAV.png
CCagn.1 by Associate
  • 810 Views
  • 0 replies
  • 0 kudos

How use SRC236 for STM32H753ZI with STM32CubeIDE

I USE STM32H753ZI and I want to oversampling some data. For IT, I use SRC236, but It send me an error. The library seems not to be adapted with the target STM32H753ZI. Has anyone encountered this problem before?Sincerely 

MYESS.1 by Associate
  • 1635 Views
  • 3 replies
  • 0 kudos