STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1549 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32H747-DISCO SWV Trace issue

Hi, I want to use SWV to profile my application which executing on CM7 core while CM4 core is disabled as it is shown on first figure. Before I start profiling I want to check if SWD work at all and I execute this command: ITM_SendChar('a');but i c...

0693W00000LyZ0PQAV.png 0693W00000LyYzqQAF.png 0693W00000LyYxfQAF.png
HTurk.1 by Associate
  • 1709 Views
  • 2 replies
  • 0 kudos

Problem with memcpy function in new IDE version

When I use memcpy like this: memcpy(&config, SavedConf, sizeof(config));whre config is an object and SavedConf is an array it turns out that nothing is copied.The problem is in version 1.9 of CubeIDE, when I compile it in 1.7 the array is copied norm...

DBrau.2 by Associate III
  • 4071 Views
  • 6 replies
  • 0 kudos

How to - bare bones startup for assembly only?

Hi All,I am new to CubeIDE, I've been playing around with it for a few days now, watching some stuff on YouTube, setting up a few modules in the CPU and making it do some basic things to get used to it all.But from here on I'd like to be able to work...

RMyer.1 by Associate III
  • 2465 Views
  • 6 replies
  • 0 kudos

Resolved! Is it possible to add custom task tags in STM32CubeIDE?

I was wondering if one could define their own task tags (special comments like the default "FIXME" or "TODO") in the IDE? The IDE is Eclipse-based, but the preferences' window is not identical. So, the guides for Eclipse, like this one (https://stack...

VVakh.1 by Associate III
  • 2354 Views
  • 1 replies
  • 0 kudos