STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Problem: STM32CubeIDE deleted all my projects inside workspace, and created new directory as per workspace choosen after renaming a folder in my PC, which was included inside workspace in STM32CubeIDE

Info: |- STM32CubeIDE 1.4.0   |- OS: Window   Description:  - I have chosen working directory/worskspace -> e.g.: C:\course_1\cubdeide_ws  - (STM32CubeIDE was closed)  - I have then renamed my course folder -> e.g.: C:\course_2\cubdeide_ws  - I the...

JAkht.1 by Associate
  • 2384 Views
  • 4 replies
  • 0 kudos

Resolved! Functions missing in FreeRTOS CMSIS v2 using STM32CubeIDE

I'm trying to use these two functions in STM32CubeIDE within FreeRTOS CMSIS v2:osKernelSuspend()osKernelResume()My goal is to put the microcontroller in STOP MODE.I get an error when compiling the project.The problem seems to be the following: the tw...

flavio23 by Associate III
  • 5447 Views
  • 7 replies
  • 1 kudos

How do I activate the FPU on F411?

I am using the F411 by CUBE IDE.I enable the CUBE's library of DSP and it was accomplished naive. Even after I inserted <include "arm_math.h"> the BUILD worked perfectly. But, after I copied one arm_FIR_filter_example from GITHUB, the compilation cha...

JSILV.2 by Senior
  • 10932 Views
  • 13 replies
  • 0 kudos

Resolved! STM32H745i-DISCO bricked no connection even with boot1

Hi, I have recently bricked my STM32H745i-disco board by turning off the m4 core within OB which had a bulk of my code. My board became unresponsive, the LCD turns white and the leds on the board light up but do not respond to the reset button. Stlin...

CChri.5 by Associate III
  • 8039 Views
  • 15 replies
  • 0 kudos

Resolved! Is it possible to debug a Makefile project into STM32CubeIDE

Hello,as the title suggests I would like to do step-by-step debugging on Makefile projects using STM32CubeIDE, however when I try to create the debug configuration it keeps showing an error message:Not able to get mcu targetReason:Build configuration...

Can I build for multiple targets on one STM32CubeIDE project?

I am currently working on a project that will use a STM32L452VET3 when the product is deployed. The PCB for the product is still being laid out, so in the meantime, I have a Nucleo board that has an STM32L452RET6 that we will use to develop and test ...

Tz.1 by Associate
  • 2044 Views
  • 1 replies
  • 0 kudos