cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling FreeRTOS and generating the code does not add osThreadNew() calls.

ROuje.1
Associate II

I am running STM32CubeIDE ver 1.11.0 and using a Nucleo-F446RE board

I create a new project and just enable FreeRTOS and add 1 task (in addition to the default task. I am using CMSIS_V2. I save and generate the code. The code for the task is there, but there are no calls in the code to create the thread. Watched some youtubes and they dont seem to do anything more than what I did, but their project have all the code there to create the threads and the threads run...

any ideas would be appreciated.

thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
gbm
Principal

See this topic for solution by Tmaniac:

https://community.st.com/s/question/0D53W00001yhWSCSA2/cubeide-111-error-while-creating-stm32f4-freertos-project

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice

View solution in original post

2 REPLIES 2
gbm
Principal

See this topic for solution by Tmaniac:

https://community.st.com/s/question/0D53W00001yhWSCSA2/cubeide-111-error-while-creating-stm32f4-freertos-project

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
ROuje.1
Associate II

I promise that I searched the forums. I even just searched for FreeRTOS and did not see this! :(

Interesting, I just set it to CMSIS_V1 and it generated the code correctly.

Still learning. Getting there :)