STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1563 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 593 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Tımer Triggered ADC+DMA+USART

/* USER CODE BEGIN 0 */void myPrintf(const char *p){uint32_t strlength1=0;uint32_t strlength2=0; const char *helpStartTextpointer=p;strlength1=0;strlength2=strlen(p);while(*p){strlength1++;*p++;} if (strlength1==strlength2 ){if(HAL_UART_Transmit_DMA(...

WhatsApp Görsel 2023-07-03 saat 00.48.22.jpg Ekran Alıntısı.JPG putty.JPG
MÖZDA.1 by Associate II
  • 1002 Views
  • 0 replies
  • 0 kudos

shifting on the written data to external flash using qspi

this is the code in the main that test the drive my stm32h750vb which is connected to the winbond25Q256jv external flash which is connected using qspi :/* USER CODE BEGIN 2 */uint8_t buffer_test[MEMORY_SECTOR_SIZE];uint32_t var = 0;CSP_QUADSPI_Init()...

Stm32

How to use timer interrupt in GPIO interrupt

M_J by Associate II
  • 4035 Views
  • 8 replies
  • 0 kudos

STM32CubeIDE locks the Workspace location. Best method to modify the Workspace location so the code base is completely portable except for the compiler/linker.

STM32CubeIDE v1.12.0This type question has been asked different ways but never specifically for a procedure. In the past we have used Eclipse Workspaces with a single project and we were able to copy, paste and rename the Workspace and then open it a...

LPM - stop mode

Hi, I am using STM32L562CEUx controller. We are using I2C,UART,SPI, RTC with external crystal(32.768MHz), external clock - 24MHz.Trying to use LPM - stop1 mode.DeInit all the peipheralsInput pins changed to Analog pins.Output pins remained sameCurren...

Pkuma.41 by Associate II
  • 814 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.