STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1304 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 525 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Missing 'External loaders' in Debugger tab

Hello,I've recently created an External Loader to be used on a TouchGFX project (H563 with SPI LCD and SPI external flash). When I use this loader in Cube Programmer, it programs the processor and SPI flash, and runs as expected. So now I want to add...

st ext ld.jpg
PP22 by Associate II
  • 862 Views
  • 4 replies
  • 1 kudos

Resolved! Debugger giving an error after uploading code

Nucleo Board STM32F401RE , STM32CubeIDE 1.19 16x2 LCD confirmed to be working using Arduino UnoHi, I am just starting with STM32 and trying to figure out my way around it after using Arduino Uno for a long time for simple projects with sensors. I ins...

No source file corresponding to 'huart2() at 0x20000108"

Edited by a ST moderator. In next time please use English language.   在STM32CUBEIDE中配置STM32F103C4完以后直接编译出现《没有 “huart2() at 0x20000108” 对应的源文件》不知道该如何把huart导入到编译器的路径下 Translation: After configuring the STM32F103C4 in STM32CUBEIDE, I encountered the...

LEGENDTU by Associate
  • 702 Views
  • 4 replies
  • 1 kudos

Error while flashing.

I am flashing a code to write into the last sector of the flash memory of STM32F401 Nucleo Board, for the first time the code was successfully dumped into the flash but while dumping it the second time this error pops up, whenever i mass erase the wh...

Screenshot 2025-11-17 150755.png

Resolved! STLink Server with MacOS 15

 Hello,I updated to Mac15 (MacOS Sonoma Public Beta), which was probably a mistake. Now I get an error from STMCubeIDE when I try to run indicating "ST-Link Server is required to launch the debug session" and to Please download it on www.st.com.  I f...

jdw by Associate II
  • 37496 Views
  • 38 replies
  • 30 kudos