STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! what causes these libc_nano.a errors?

Description Resource Path Location TypeC:/ST/STM32CubeIDE_1.18.0/STM32CubeIDE/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.win32_1.0.0.202411081344/tools/bin/../lib/gcc/arm-none-eabi/13.3.1/../../../../arm-none-eabi/li...

carlesls2 by Associate III
  • 4798 Views
  • 5 replies
  • 2 kudos

STM32U073/083 I2C4, not visible in SFR view

HiI'm using the stm32u073, the i2c4 peripheral registers are not visible in the SFR view when debugging, and the peripheral address is not included in the reference manual table 4.I checked the .svd for u83, is the same.Cheers  

max34000 by Associate
  • 1065 Views
  • 2 replies
  • 0 kudos

Received Data length is wrong in usb Communication

"static uint8_t USBD_CDC_DataOut(USBD_HandleTypeDef *pdev, uint8_t epnum)"In stm32u575 controller and in this function while I am calling"uint32_t receivedLength = USBD_LL_GetRxDataSize(pdev, epnum);" it gives me 1 insted of 6 or 5 bytes I am recivin...

Sarathk3k by Associate II
  • 1892 Views
  • 3 replies
  • 0 kudos

STM32 AudioSoundDetector example

Im trying to run the ADF_AudioSoundDetector example from one of the example list of B-U585I-IOT02A board i generated code from cubeMX of this example. i did not change the ioc files when i try to open the project from stm32cubeide to run it, nothing ...

jzzunn by Associate II
  • 1180 Views
  • 1 replies
  • 0 kudos

ETH PHY Address problem for old and new Cubeide

 Hi, I have a problem. when I used old cube ide version, ı can changing physical address and ethernet module is to take ip address. But when I use new version I want to edit phy address but this area is not in new version.That's why I can't use the E...

kadirsrht by Associate II
  • 2766 Views
  • 4 replies
  • 2 kudos