STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 227 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4070 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB5MMGH6TR USB serial port (COM)

Good morningI must project a board in this way:This baord will be connect to usb -c of the computer.There will be a converter 5V --> 3.3V.A MCU with bluetooth and antenna integrated.The goal is: the computer must recognize the board like USB serial P...

In version 1.4.1, which ZAP tool is being used

When using the version v2024.08.14-nightly described in the Wiki, configuring and outputting with the ZAP tool does not include GeneralCommissioning inside DispatchSingleClusterCommand in IMClusterCommandHandler.cpp. This causes a build error.Could y...

Stop and restart via LPTIM

Good morning,I am working with the MB1389E board and STM32CUBEIDE. I need to put it into low power mode for a few minutes and then measure and transmit data when it wakes up.I tried the LPTIM_Timeout example (included in the STM32Cube MCU Package exa...

UmbertoL by Associate
  • 365 Views
  • 1 replies
  • 0 kudos

Resolved! Flashing M0+ Core with Zigbee RFD Firmware on STM32WB55

 Dear ST Community, I'm working on a Zigbee IoT project where I need to configure my STM32WB55RG Nucleo board as a Zigbee End Device that joins an external coordinator (Raspberry Pi + CC2531 running Zigbee2MQTT). I'm having trouble properly flashing ...

Azizzr02 by Associate II
  • 1225 Views
  • 3 replies
  • 0 kudos

stm32wb55rev6

i am using the stm32wb55rev6.how can we able to drive the rf transmit mod external power amplifier (PB0) to control the rf.Is there any other things we should do in the cubemx other than enabling the rf?please share the document if it is there.

TejasK by Associate III
  • 751 Views
  • 3 replies
  • 0 kudos

STM32WL3 status when wakeup from deep sleep not working

1. [Part Number] STM32WL33CC12. [Environment] Windows OS, STM32CubeIDE version 1.18.0, Firmware package STM32Cube FW_WL3 V1.1.03. [Schematics] STM32 Nucleo-64 development board4. [Details] See below.5. [Expected behavior] When the device is woken up ...

ola by Associate III
  • 3095 Views
  • 7 replies
  • 4 kudos