STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! not able to connect to the stm32cube monitor rf.

i am usng stm32wb55rev6 microcontroller for my project. I updated the firmware upgrade service to the latest version of the v2.1.0.0 and updated the stack version to the latest version of v1.23.0.3.Still i am not able to connect to the stm32cube moni...

TejasK_0-1755520705766.png TejasK_1-1755520723599.png
TejasK by Associate III
  • 1446 Views
  • 7 replies
  • 0 kudos

FUS_IMAGE_ERSERROR from FUS while FW upgrade

Hi there,On a STM32WB55RG, I would like to write a routine in my firmware to upgrade the wireless firmware through the FUS mailbox.I'm able to exchange request/response through the mailbox, for instance, at startup FUS_GET_STATE returns FUS_STATE_IDL...

rmedaer by Associate II
  • 827 Views
  • 6 replies
  • 0 kudos

STM32 WL55JC1 FUOTA

Good morning, I have been trying to integrate FUOTA for a few days in my Nuclo STM32 WL55JC1 project. Starting from the provided example STM32CubeWL_FW_1.3.1 from MXCube, if I try to build in CubeIDE I get the following error:   make[1]: *** No rule ...

IngSerio by Associate III
  • 1943 Views
  • 4 replies
  • 0 kudos

Resolved! Cannot run any example on Nucleo-WB55RG board

Hello @STTwo-32,I was having the same issue and pressing the "start wireless stack" button did the trick for me. I was assuming after flashing the FUS & BLE Stack firmware, is that the CPU2 would be up and running already. So, does this mean that we ...

Jopail12 by Associate II
  • 924 Views
  • 2 replies
  • 1 kudos

STM32WB5MMG Ble connection problem

Hello!I have an STM32WB5MMG with a breakout board (more specifically Sparkfun ATP breakoutSparkFun MicroMod ATP Carrier Board - DEV-16885 - SparkFun Electronicswith the STM32WB5MMG module SparkFun MicroMod STM32WB5MMG Processor - DEV-21438 - SparkFun...

DLid1_0-1693668323949.png DLid1_1-1693668411009.png DLid1_2-1693668604268.png address.png
DLid.1 by Associate II
  • 7556 Views
  • 7 replies
  • 0 kudos

Resolved! NUCLEO-WL55JC stop mode consumption

Hi everyone , I'm testing ultra-low power on the NUCLEO-WL55JC using STM32CubeIDE . My goal is to reach ~0.9 µA in Stop 2 mode, but I consistently measure around 2.9 mA, even with the debugger disconnected. My setup: Stop 2 mode enabled MSI @ 100 kHz...

marouax by Associate II
  • 1507 Views
  • 4 replies
  • 1 kudos