NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Greetings,STM32WLE5 reference manual says an external TCXO should have a sinusoidal output. Clipped sine oscillators seem to be more available, do you think they would work too?Thanks!
I have my custom STM32WB55CE board. I had programmed the example code "EEPROM_Emul" from"X-CUBE-EEPROM_V2.0.0" package on it. It was working fine. Then I did FUS upgrade with BLE full stack binary programming on it. After that, the same EEPROM emulat...
Hello, I ask here a question already asked in another topic and which as not received any answer.**** I would like to know how toimplement Multicast messagingon my end-node (currently using Murata Module (CMWX1ZZABZ-078) with ST LoRalibraries (Expans...
Hi All:I try to upgrade RF stack by usb/swd interface on p-nucleo-wb55, and the attach file contain the command I use.I found that the stack get errors, after upgrading the stack by swd interface?Then, the usb interface can't access again...swd...
Hello,Currently our team is working with "STM32WB55 P-NUCLEO-WB55 Platform", we were able to flash the stack.Then we have tried the same ZigBee project and able to self-demonstrate the same successfully, like led on/off and sending messages.As our te...
Hi all,From Nucleo STM32WB55 to my own application with the same micro.I have written an application based on Cable Replacement Service from examples. I did my PCB and everything works.Now I have to add my own bootloader with cipher. Beacause of this...
Hello Everyone, I have brought newly launched NUCLEO-64 board which have built in LoRa SOC with STM32WL55JC2 architecture mcu. Though the board is newly launched, I am unable to find any documents or example to establish point to point lora communica...
STM32WLE5CC REFERENCE SCHEMATIC OR DEVELOPMENT BOARD SCHEMATIC I NEED MAJORLY LORA ENABLED ANTENNA INTERFACE I AM PLANNING TO USE THIS ICS IN ONE OF MY PRODUCT. SO GUIDE ME IN HARDWARE SUPPORT
Hi,Need a support for STM32WL5CC development on Software and Hardware schematic level.
I developed a LoRa device with STM32L072RZ+SX1272MB2xAS. The device could send data every 40 s and It's working well. But the problem happened when a Lora network has devices with more than 10 nodes. The problem is sometimes devices can't send any da...