STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! why targeting STM32WL as end node instead of STM32LO?

I bought p-nucleo lrwan2 working with STM32LO MCU,and i'am wondering to configure its device sensor as end node ,watching the last video posted by ST they were working with the same pack but they targered STM32WL as end node instead of working with t...

Zbenj.1 by Associate II
  • 2504 Views
  • 5 replies
  • 0 kudos

Problem with LoRaWAN and DAC in the same time.

Hi guys. When I program the device with LoRaWAN and DAC with pin extern (PA10), I saw in oscilloscope that DAC stay high every when has uplink. Like the image: Does anyone have any idea why this happens? Thanks!

0693W00000BcMkHQAV.jpg
MRebo.1 by Associate II
  • 2110 Views
  • 5 replies
  • 0 kudos

Using stm32wb core M0+ for user program

Hi,I am looking for a dual core controller and options I have been able to find out are:Stm32Wb seriesStm32H seriesBeing, H series quite expensive, Is it possible to use WB series M0+ for running another application in parallel?Or we can only use it ...

AKuma.33 by Associate II
  • 1576 Views
  • 1 replies
  • 0 kudos

OB IPCC shifted left vs pMBTable

I set the OB bit to 0xe4, but it shifts left 1 on flash with IDE. MAPPING_TABLE 0x00000000200000e4  0x13c load address 0x0000000008003744 MAPPING_TABLE 0x00000000200000e4  0x13c MbMux/mbmuxif_sys.o    0x0000000020000220    . = ALIGN (0x4)0x000000002...

bblouin by Associate III
  • 729 Views
  • 0 replies
  • 0 kudos

Resolved! Lora RN2903a with STM32F745 .. when transmitted system commands the uart receive is shown below .set the baud to 57600 bps and DMA in circular for half word .

There is something missing upon receiving junk .How do we keep the count of how much response will be received in advance ? should any flags be set to check whether the response received is correct and clear upon not receiving proper response , bit ...

SG.4 by Associate II
  • 3368 Views
  • 4 replies
  • 0 kudos