STM32wbxx_hal_smartcard not fully working in v1.10
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-11-23 7:49 AM
Hi,
We've just updated our HAL from 1.6 to 1.10 and encountered some issues with our link to secured element.
ATR is successfully received.
After any transmit (we are using DMA), a call to a receive return BUSY.
We get file STM32wbxx_hal_smartcard.c back to v1.6 and applied diff one by one, and some lines made the difference.
Here is the diff with minimal git chunks to works:
iff --git a/Drivers/STM32WBxx_HAL_Driver/Src/stm32wbxx_hal_smartcard.c b/Drivers/STM32WBxx_HAL_Driver/Src/stm32wbxx_hal_smartcard.c
index 22f84da1..52bafae6 100644
--- a/Drivers/STM32WBxx_HAL_Driver/Src/stm32wbxx_hal_smartcard.c
+++ b/Drivers/STM32WBxx_HAL_Driver/Src/stm32wbxx_hal_smartcard.c
@@ -823,23 +823,14 @@ HAL_StatusTypeDef HAL_SMARTCARD_Transmit(SMARTCARD_HandleTypeDef *hsmartcard, ui
/* Disable the Peripheral first to update mode for TX master */
CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* In case of TX only mode, if NACK is enabled, the USART must be able to monitor
- the bidirectional line to detect a NACK signal in case of parity error.
- Therefore, the receiver block must be enabled as well (RE bit must be set). */
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX)
- && (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
- {
- SET_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
- }
- /* Enable Tx */
+ /* Disable Rx, enable Tx */
+ CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
+ SET_BIT(hsmartcard->Instance->RQR, SMARTCARD_RXDATA_FLUSH_REQUEST);
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_TE);
/* Enable the Peripheral */
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* Perform a TX/RX FIFO Flush */
- __HAL_SMARTCARD_FLUSH_DRREGISTER(hsmartcard);
-
hsmartcard->ErrorCode = HAL_SMARTCARD_ERROR_NONE;
hsmartcard->TxXferSize = Size;
hsmartcard->TxXferCount = Size;
@@ -854,28 +845,19 @@ HAL_StatusTypeDef HAL_SMARTCARD_Transmit(SMARTCARD_HandleTypeDef *hsmartcard, ui
hsmartcard->Instance->TDR = (uint8_t)(*ptmpdata & 0xFFU);
ptmpdata++;
}
- if (SMARTCARD_WaitOnFlagUntilTimeout(hsmartcard, SMARTCARD_TRANSMISSION_COMPLETION_FLAG(hsmartcard), RESET, tickstart,
- Timeout) != HAL_OK)
+ if (SMARTCARD_WaitOnFlagUntilTimeout(hsmartcard, SMARTCARD_TRANSMISSION_COMPLETION_FLAG(hsmartcard), RESET, tickstart, Timeout) != HAL_OK)
{
return HAL_TIMEOUT;
}
-
- /* Disable the Peripheral first to update mode */
- CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX)
- && (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
+ /* Re-enable Rx at end of transmission if initial mode is Rx/Tx */
+ if (hsmartcard->Init.Mode == SMARTCARD_MODE_TX_RX)
{
- /* In case of TX only mode, if NACK is enabled, receiver block has been enabled
- for Transmit phase. Disable this receiver block. */
- CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
- }
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX_RX)
- || (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
- {
- /* Perform a TX FIFO Flush at end of Tx phase, as all sent bytes are appearing in Rx Data register */
- __HAL_SMARTCARD_FLUSH_DRREGISTER(hsmartcard);
+ /* Disable the Peripheral first to update modes */
+ CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
+ SET_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
+ /* Enable the Peripheral */
+ SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
}
- SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
/* At end of Tx process, restore hsmartcard->gState to Ready */
hsmartcard->gState = HAL_SMARTCARD_STATE_READY;
@@ -996,23 +978,14 @@ HAL_StatusTypeDef HAL_SMARTCARD_Transmit_IT(SMARTCARD_HandleTypeDef *hsmartcard,
/* Disable the Peripheral first to update mode for TX master */
CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* In case of TX only mode, if NACK is enabled, the USART must be able to monitor
- the bidirectional line to detect a NACK signal in case of parity error.
- Therefore, the receiver block must be enabled as well (RE bit must be set). */
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX)
- && (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
- {
- SET_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
- }
- /* Enable Tx */
+ /* Disable Rx, enable Tx */
+ CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
+ SET_BIT(hsmartcard->Instance->RQR, SMARTCARD_RXDATA_FLUSH_REQUEST);
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_TE);
/* Enable the Peripheral */
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* Perform a TX/RX FIFO Flush */
- __HAL_SMARTCARD_FLUSH_DRREGISTER(hsmartcard);
-
/* Configure Tx interrupt processing */
if (hsmartcard->FifoMode == SMARTCARD_FIFOMODE_ENABLE)
{
@@ -1153,23 +1126,14 @@ HAL_StatusTypeDef HAL_SMARTCARD_Transmit_DMA(SMARTCARD_HandleTypeDef *hsmartcard
/* Disable the Peripheral first to update mode for TX master */
CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* In case of TX only mode, if NACK is enabled, the USART must be able to monitor
- the bidirectional line to detect a NACK signal in case of parity error.
- Therefore, the receiver block must be enabled as well (RE bit must be set). */
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX)
- && (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
- {
- SET_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
- }
- /* Enable Tx */
+ /* Disable Rx, enable Tx */
+ CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
+ SET_BIT(hsmartcard->Instance->RQR, SMARTCARD_RXDATA_FLUSH_REQUEST);
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_TE);
/* Enable the Peripheral */
SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- /* Perform a TX/RX FIFO Flush */
- __HAL_SMARTCARD_FLUSH_DRREGISTER(hsmartcard);
-
/* Set the SMARTCARD DMA transfer complete callback */
hsmartcard->hdmatx->XferCpltCallback = SMARTCARD_DMATransmitCplt;
@@ -2980,22 +2944,15 @@ static void SMARTCARD_EndTransmit_IT(SMARTCARD_HandleTypeDef *hsmartcard)
CLEAR_BIT(hsmartcard->Instance->CR3, USART_CR3_EIE);
}
- /* Disable the Peripheral first to update mode */
- CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX)
- && (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
+ /* Re-enable Rx at end of transmission if initial mode is Rx/Tx */
+ if (hsmartcard->Init.Mode == SMARTCARD_MODE_TX_RX)
{
- /* In case of TX only mode, if NACK is enabled, receiver block has been enabled
- for Transmit phase. Disable this receiver block. */
- CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
- }
- if ((hsmartcard->Init.Mode == SMARTCARD_MODE_TX_RX)
- || (hsmartcard->Init.NACKEnable == SMARTCARD_NACK_ENABLE))
- {
- /* Perform a TX FIFO Flush at end of Tx phase, as all sent bytes are appearing in Rx Data register */
- __HAL_SMARTCARD_FLUSH_DRREGISTER(hsmartcard);
+ /* Disable the Peripheral first to update modes */
+ CLEAR_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
+ SET_BIT(hsmartcard->Instance->CR1, USART_CR1_RE);
+ /* Enable the Peripheral */
+ SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
}
- SET_BIT(hsmartcard->Instance->CR1, USART_CR1_UE);
/* Tx process is ended, restore hsmartcard->gState to Ready */
hsmartcard->gState = HAL_SMARTCARD_STATE_READY;
Labels:
- Labels:
-
STM32Cube MCU Packages
-
STM32WB series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0