STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

WB5MMG RTC Inaccurate

WB5MMG RTC Inaccurate, RTC increase by 1s requires 10s or more in reality.32.768 LSE has been used. RTC_TimeTypeDef sTime = {0}; HAL_RTC_GetTime(&hrtc, &sTime, RTC_FORMAT_BIN); RTC_DateTypeDef sDate = {0}; HAL_RTC_GetDate(&hrtc, &s...

0693W00000HpcCBQAZ.png 0693W00000HpcCeQAJ.png
Csu.11 by Associate II
  • 3227 Views
  • 7 replies
  • 0 kudos

STM32wl55 subghz linker error using cubemx

Hi there,I want to run some commands and get results on our custom designed STM32wl55 PCB. I started the project using cubemx but there is a subghz linker error.Could you please help me how to solve it?ThanksError: L6218E: Undefined symbol HAL_SUBGHZ...

SK.20 by Associate
  • 4387 Views
  • 9 replies
  • 0 kudos

HAL_ADC_ConvtCpltCallback not getting triggered

Working with the STM32WB5MM.My intent is to trigger a one shot ADC/DMA combo that will read a bunch of pins with heavy oversampling, then trigger a callback for the processor to deal with later.Core Clock is 32Mhz, ADC clock is 1MhzI've got the ADC D...

JWieb by Associate III
  • 2360 Views
  • 1 replies
  • 0 kudos

Resolved! How to enable FPU on STM32WL?

Mates,   I am new in the environment of STM32. Now, I have a problem with a DSP application.   I'd like to use FFT functions on STM32WL55 board. However, when I try to use CMSIS built-in functions, the project can not be built, it gives VFP errors.  ...

Resolved! Struggling to get UART debug printer to work with fresh MX Build.

I build a new application with a custom GATT and would like to use the UART debug features that can be seen in the examples. I configured my IOC as follows and verifid the UART is working with the following code: char msg[] = "Begin1\n"; HAL_UART_...

0693W00000HpiYqQAJ.png
JWieb by Associate III
  • 1312 Views
  • 1 replies
  • 0 kudos

Get UID and use it in BLE Local Name

Hi,I am using the STM32WB55 and would like to use part of the chip's unique ID as part of the local name in my BLE application.I was hoping someone could easily show me how I could do this, or at a minimum, get the UID?Thanks for any help.

kcire L. by Associate III
  • 3359 Views
  • 4 replies
  • 0 kudos

Resolved! I2C3 issue on NUCLEO STM32WL using CubeMX : I2C1 working well

Hello, I have a problem to use another bus (I2C2 or I2C3) than the I2C1 bus in the nulceo STM32WL55JC1My code is working with I2C1 but when I just change hi2c1 into hi2c3. Then, HAL_I2C_Mem_Write() is no longer working. I cannot see any signal with a...

0693W00000Ho8XQQAZ.png 0693W00000Ho8XfQAJ.png 0693W00000Ho8X1QAJ.png 0693W00000Ho8WwQAJ.png
LLr.1 by Senior
  • 5266 Views
  • 5 replies
  • 0 kudos