cancel
Showing results for 
Search instead for 
Did you mean: 

Do I have to use a 32 kHz oscillator (LSE) for the STM32WB55 MCU ZigBee application?

Batuhan A.
Associate II

Hello,

I am going to use a 32 MHz oscillator (LSE) for a ZigBee application on STM32WB55. Do I have to add a 32 kHz oscillator? I do not need RTC.

Best regards,

Batuhan

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

You can use the STM32WB55 without the LSE if you:

  • don't need an RTC and
  • don't need beaconing support and
  • don't want to synchronize internal oscillators from LSE

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

You can use the STM32WB55 without the LSE if you:

  • don't need an RTC and
  • don't need beaconing support and
  • don't want to synchronize internal oscillators from LSE

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.