NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Good morning,I have been following the stm channel board videos on the LoraWan examples. I was able to correctly configure and connect the board from the example provided in the MX “LoRaWan_EndNode”.But replicating the last video:https://www.youtube....
Hello,I intend to develop an application using the STM32WB and a Telit LTE module (TX62). I would like to know if there is a way for me to use the LTE module to update the firmware of the STM32WB remotely. Can this be done via UART communication betw...
Hi,While building the example FUOTA code from icubelrwan software expansion. I am facing "No rule to make target error" attached the screenshot. Tried to build after including the path of the folder but still facing the same error. attached the scree...
I am currently working with a stm32wl55JCI and using RTOS. I am currently running into overflow errors of ram1. I am currently using an example project using RTOS. I tried using heap5 and used the sample templates for how to define the memory regions...
Hi, I am setting up an ble audio project with STM32CubeIDE。There is no ble audio choose with STM32_WPAN view in STM32CubeMX。I just can select the ble choose that is Starts from a skeleton project with host stack & GAP and GATT initialization。 ...
Hello,Could you tell me how can i enable clock access to SYSCFG in STM32WB55RG board, because i couldn't find the proper bit to enable SYSCFG in APBENR registers in the reference manual
I think you guys have an issue here with your return in aci_gap_slave_security_req_rp0.Command itself works fine, as android does show a Pair Request. But I get a error on the Status response. Looking in documents it is ACI_GAP_PERIPHERAL_SECURITY_R...
Hello STM32 Community,I hope you're all doing well. I'm reaching out regarding a project we're developing using the STM32WL5MOCH6TR microcontroller. Our project requires the use of the Mbus stack protocol for communication purposes.However, when atte...
Hello again, I'm using STM32WB, the name and the image of HeartRate service is visible on my mobile device but I can't set the name and the image for my own service which I create it Why?
Hi,We are evaluating using the Nucleo-WB55RG with Matter for a project. This would require being able to commission and interact with the device from Google Home using a Google Nest device as the border router. We are unable to setup the device in G...