NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I want to write a very simple program that sends a packet using BLE_LLD. For simplicity sake, for now, I prefer not using sequencer and put everything in the main loop.According to UM2804, I should be able to do that only using HAL interfaces. I star...
I'm having a problem in a 1 gram tracker that uses an stm32wle5 powered by a 2.4V LTO battery and 4mW solar cell (through bq25504 energy harvesting chip). If the battery discharges below 1.7V ("should never happen"...) the solar cell cannot recharge ...
I am customizing the LoRaWAN_End_Node example for our purpose. My application is pretty simple, I send unconfirmed uplinks every 5 minutes after a successful join. On successful uplinks, I get MCPS-Confirm with a status of LORAMAC_EVENT_INFO_STATUS_O...
Hi,When creating a custom template BLE app in CubeMX everything works fine while not changing the UUID of service1, it builds and compiles well. But if I change the UUID to my own UUID (with UUID 128 input type to full), after generating the new code...
I made a Demo using STM32WB5MMG to communicate with USB dongle or phone (BLE notification),AND I collect data from the MAX30001 (two interrupt pins PC10 and PC11, SPI1 communication) and the MAX30112 chip (interrupt pin PD0, I2C3 communication) by tr...
The STM32WL55 JC modules are taking 4 seconds time to switch from Receiver mode to transmitting mode, can you please give some information that how can i reduce that switching time. https://github.com/stm32-hotspot/STM32WL-SubGHz-Phy-Rx-Hop Used th...
I have succesfully implemented my own BLE advertisement (LEGACY) using the STM32WB55 MCU.I have attached my code below.In a nutshell I have created three timers and two tasks.When the Heartbeat timer expires it calls the Heartbeat function:This then ...
Hello,We are trying to use MTU larger than 24X bytes.The characteristic size set to 483 bytes (CFG_BLE_MAX_ATT_MTU).We tried to use aci_gatt_update_char_value_ext to set the value (as the HCI layer is limited to 255 bytes transfer).aci_gatt_update_ch...
I am using STM32WB for My Application, I want to initailly mcu is stop mode or sleep mode,when external interrupt (switch) is triggered its wakeup from low power mode.After wake up re-installize the System Clock for Mcu running configured ...
Hello,I am trying to use B-L072Z-LRWAN1 kit with library from Semtech which is Firmware Driver and LoRaWAN Stack V4.1.0. I solved error step by step with adding files one by one. Now that error occurs after Debug program. I am using Ubuntu Disco Ding...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.