NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm having some issues with the STM32WB06 when trying to achieve low power consumption. I hope someone can help me solve these problems.Issue 1: After initializing the Bluetooth protocol stack and enabling automatic connection establishment, it c...
Hi everyone,I am encountering a HCI_HARDWARE_ERROR_EVENT with code 0x02 (BlueCore time overrun error) on STM32WB devices.Key observations:Issue is observed only on some units, while others operate normallyAll devices use the same firmware, BLE stack,...
We are a bachelor project group developing a BLE Direction Finding handheld "tracking compass" using AoA on STM32WB09 devices.We have reached a stage where BLE communication, CTE reception, antenna switching, and IQ report generation all appear funct...
Hi, I'm searching for the best Rx sniff mode as suggested in AN6362: I'm able to use carrier sense (RSSI_THR, CS_F interrupt) and SQI (SQI_THR, SYNC_VALID_F interrupt) but PQI never works.The MCU is in WFI state, sequencer not used.I have changed th...
MCU : STM32WLE5CCU6STM32CubeIde version : 2.1.1STMC32CubeMx version : 6.17.0Firmware Package Name and Version : STM32Cube FW_WL V1.5.0Application : FUOTA using LoRaWANSetup : End Node(STM32WL) <===> Gateway(Dragino LPS8) <====> TTNHello everyone,Befo...
Hardware: STM32 NUCLEO-WB15CC (STM32WB15CCUX) RTOS: FreeRTOS BLE stack: STM32WB WPAN / BLE via CPU2 (M0+) Hi, When writing a small configuration block (~48 bytes) to the internal Flash from CPU1 (M4 FreeRTOS task), the BLE connection drops immedi...
I have an STM32WBA data logging project loosely based on the BLE heart rate project. I sync the RTC via either a BLE message, or NTP from a serial modem. All good; works well and the RTC timestamp ticks along whilst the code is in stop2 sleep. The de...
void HAL_MRSubG_IRQ_Callback(void) { uint32_t irq = __HAL_MRSUBG_GET_RFSEQ_IRQ_STATUS(); if (irq & MR_SUBG_GLOB_STATUS_RFSEQ_IRQ_STATUS_RX_OK_F) { last_rx = HAL_GetTick(); HAL_GPIO_WritePin(LD1_GPIO_Port, LD1_Pin, GPIO_PIN_SET); if (H...
Hi, I'm using the STM32WBA54KG microcontroller to comunicate by BLE. In STM32CubeMX (v6.13.0), I have actived the STM32_WPAN packet and the configuration "USE_TEMPERATURE_BASED_RADIO_CALIBRATION" is "YES".I need to read the Vcore channel to know if t...
Environment:MCU: STM32WB09KE, Cortex-M0+Board: NUCLEO-WB09KEIDE: STM32CubeIDE 2.1.0STM32CubeIDE Build: 27993_20260219_1630 (UTC)STM32CubeMX Version: 6.17.0OS: Windows 11 HomeFirmware package: STM32Cube_FW_WB0_V1.4.0Example project used: BLE_Direction...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.