STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Hello everyone, I am interfacing stm32f103 to LCD44780 to display character in one location (1,1) but it shows in whole pixel 16x2. could you give me idea ?

here is my code void LCD_Enable(){HAL_GPIO_WritePin(GPIOB,GPIO_PIN_14,1);HAL_Delay(1);HAL_GPIO_WritePin(GPIOB,GPIO_PIN_14,0);HAL_Delay(1);}void LCD_Send4Bit(unsigned char Data){HAL_GPIO_WritePin(GPIOA,GPIO_PIN_8,Data&0x01);HAL_GPIO_WritePin(GPIOA,GPI...

Bunty Gtm by Associate II
  • 1041 Views
  • 0 replies
  • 0 kudos

Resolved! Touchgfx::BoxWithBorder constructor

Hi,I don't get why I can't set the border thickness/color directly when creating the BoxWithBorder object._boxWithBorder3(50, 50, touchgfx::Color::getColorFrom24BitRGB(150, 150, 250), touchgfx::Color::getColorFrom24BitRGB(0, 0, 0), 5,50)Indeed, it do...

GMeur by Senior II
  • 1396 Views
  • 2 replies
  • 0 kudos

STemWin Touch Driver (ADS7843) problem

Hello All,I am setting up STemWin on STM32F103VE MCU. The graphical part is all setup and working fine!The problem is the Builtin touch screen driver of STemWin. I have gone through the manual and created the low level SPI communication part and test...

0690X000008wKHsQAM.jpg

Resolved! How to create a blocking message box in touchGFX?

We have an existing embedded application with older GUI which is being ported to TGFX. For keeping the old logic, we want to display a blocking message box and wait for user response (button click) in a widget callback(GUI button callback). The probl...

zzzzz by Senior
  • 6492 Views
  • 14 replies
  • 0 kudos

STemWim is precompiled with wrong endianness ?

Hi, I am using STemWin on a ST32F429 in combination with a ST7735S connected to the cpu over an 8 bit interface. My pixel are 16 bit with color format RGB=565. My controller expects the bytes to be transferred R5G3, G3B5.The problem I am running into...