STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Get an example TouchGFX

I wanted to use the example "Method 1 - From GUI task" TouchGFX. I downloaded PollDemoHwInt 4.9.3.zip. Unpacked. Can't open STM32CubeIDE 1.1.0?

AD�?b by Senior
  • 995 Views
  • 4 replies
  • 0 kudos

Resolved! Processor Load calculation and (perhaps) display

The emWin demos show a processor load value on the screen, is there already a method defined for this in the TouchGFX / FreeRTOS configuration. I need to know how "near the edge" I currently am. It will help to know if I have enough processor HP to c...

Multiple Definitions Errors

I am getting compiling errors when trying to include a custom class into a TouchGFX project.I made a class called "test" with it's test.h and test.cpp components.//File: test.h   #pragma once class test { public: test(); ~test();   void s...

TLahr.1 by Associate III
  • 3139 Views
  • 5 replies
  • 0 kudos

Is the LCD display on 32F469IDISCOVERY removable?

I would like to buy an evaluation board for the STM32F469 chipset but am trying to use it with a circular display. Can I easily remove the LCD screen it comes with and use my own or is there another eval board that you can buy without a screen attach...

BSunw.1 by Associate III
  • 1722 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE not link library files correctly

when i build a project with the .a lib. the problem"make: *** [makefile:47: freertos-stemwin.elf] Error 1"make -j4 all" terminated with exit code 2. Build might be incomplete."was happened.told me that"d:\program files\stm32cubeide_1.1.0\stm32cubeide...

0690X00000BvpxCQAR.png 0690X00000BvpxgQAB.png 0690X00000BvpyUQAR.png 0690X00000BvpyeQAB.png
zpeng.11 by Associate
  • 2824 Views
  • 2 replies
  • 2 kudos