STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Animated images with thousands of .PNGs slows down a TouchGFX Designer. Looking for alternative approaches.

Hello, I’m working on device equipped with STM32H753 and LCD (320x240), 16 MiB of SDRAM (available for caching will be about 13 MiB) and SD card (SDMMC interface) that will be used also for storing images for TouchGFX.In some cases device shall disp...

scott.sp by Associate II
  • 2000 Views
  • 3 replies
  • 0 kudos

FMC and Code Generation Issue

Hi,I am developing an application running on STM32F469 MCU to control an LCDGenerating my Code using STM32CubeMX.Using FMC Memry type is LCD_Interface, A23 Data: 16 bitsThe bug I found is in the STemwin_wrapper.c file, in functions : FMC_BANK_WriteD...

JKhal by Associate III
  • 1374 Views
  • 1 replies
  • 0 kudos

Resolved! Hard Fault

Hello,I am developing an app using tortoise git, I have made a lot of commit and cleanup in rep and my application was ok.Ten commits ago I never made a clean up, so, when I cleaned up the repository my app crash in one line of code I made before.I ...

MPJEG video demo for STM32F746G-DISCO?

This post (https://touchgfx.zendesk.com/hc/en-us/community/posts/115000138705/comments/115000702685 ) mentions a demo for an MJPEG video player in TouchGFX.The link is given as:http://ftp.draupnergraphics.com/TouchGFX/demos/simple_video769eval.zipNo...

Resolved! TouchGFX for Nucleo boards

Is it possible to implement touchgfx with a NUCLEO board. I think yes because my NUCLEO STM32F767NI has LTDC.But i doubt because the aren't touchgfx templates for nucleo boards.

AMerc.4 by Senior
  • 1339 Views
  • 3 replies
  • 0 kudos

TouchGFX, STMCube, Converting to Double buffering

I have a Newhaven 800x480 display connected to the STM32F746G-DISCO board.Finally got the display and the touch working. It is currently using a single buffer @ 0xC0000000 SDRAM.There is some artifacts when the screens change with the cover process....

MEder by Associate III
  • 1834 Views
  • 3 replies
  • 0 kudos