STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! What is handleTickEvent() period?

Hi,This is the code snippet to animate containerAF1:void mainScreenView::handleTickEvent() { static uint32_t startMove = 0; startMove++; bool pr; if(startMove<40) pr = true; else pr = false; containerAF1.setVisible(pr); containerAF1.invalidate(); if(...

RGajd.1 by Associate II
  • 2044 Views
  • 2 replies
  • 0 kudos

How to change animation speed in swipecontainer? And Can I get the current selected page index in swipecontainer?

[Q1] I have 3 pages in a swipecontainer in my program. One of them is a watch face and when I swipe a page to this watch face page, the speed of animation is too slow. So I want to change the speed of animation faster. [Q2] And I want to get the curr...

JPark.14 by Associate III
  • 2385 Views
  • 4 replies
  • 0 kudos

using custom container on multiple page

I am trying to use a custom container to create a master menu button list to change pages, it looks like it is all working but when the toggle button from the custom container are selected to change page it reset to default states when i change page...

BCabo.1 by Associate
  • 2069 Views
  • 3 replies
  • 0 kudos

Can anyone suggest me 8" to 10" TFT LCD + Capacitive Touch screen with MIPI DSI interface which can be directly connected to STM32F469I-Discovery Board?

Hi Guys,I want to connect 8" to 10" TFT LCD + Capacitive Touch Screen display with MIPI DSI interface to STM32F469I-Discovery just by removing the existing 4" TFT LCD. I had searched in the internet and I didn't get any TFT LCD CTP with MIPI DSI inte...

SK S.1 by Associate III
  • 6128 Views
  • 11 replies
  • 0 kudos

Main screen and setting screen

I want to create a parameter setting screen in addition to the main screen.Read the state of the switch at startup to determine which screen to display.I want to dynamically decide the display screen like this. How should I create it?Do you have samp...

Ebun.1 by Senior
  • 2121 Views
  • 4 replies
  • 0 kudos

Resolved! Frame buffer in internal RAM is empty

Hi,I have a custom board setup using a display connected via SPI and I've used the example code from the STM32L496G-DISCO board as a reference.My SPI display driver works correctly as I am able to send data directly to the display and show it on the ...

SThon.1 by Associate II
  • 3295 Views
  • 5 replies
  • 0 kudos

Analog and Digital in the same pin

sorry for my englishI have a LCD TFT 480x320 with touch, and the pins like for the arduino. He is working very fine with STM32F407ZG, its all OK, I converted MCUFRIEND_KBV, with help from developer, to stm32. But i need to use the touch, but theprobl...

MSilv.1 by Associate III
  • 2741 Views
  • 5 replies
  • 0 kudos