STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Combine font files for TouchGFX (western + chinese)

Hi,Does anyone know how to combine western + chinese + japanese fonts into one file for TouchGFX designer?My problem is that I want to use Source Sans Pro font, which does not have chinese, japanese etc. I want to combine Source Han Sans with it, whi...

Tuoman by Senior II
  • 2458 Views
  • 6 replies
  • 0 kudos

Resolved! Touch can not initialize HAL

Touch Designer set pix format as ARGB2222, RGB LCD using LTDC setted pix format as L8. In a simple project ,now it can show correctly. But I imgrate this project with a Touch Designer Demo Project , it can not work correctly. Error show I found uint1...

0693W000001rFiSQAU.jpg 0693W000001rFjLQAU.jpg
Breeze1 by Associate III
  • 2250 Views
  • 5 replies
  • 0 kudos

Resolved! TouchGFX 4.12.3 does not work

Thank you for helping.STM32F746G DISCO with Application TemplateBlank UI with UI TemplateWhen you create it with this, the following display appears.Creation of TouchGFX Application failedWhat is the cause?Is there a log to analyze the cause?Thank yo...

Ebun.1 by Senior
  • 1494 Views
  • 4 replies
  • 0 kudos

Interfacing LCD 4-bits mode with stm32F103RBT6

#include "stm32f10x.h" // Device header #include "LCD.h" #include "stdint.h" #include <stdio.h>     void GPIO_Init(void) { // Port B is used for I2C1 communication : SCL1-->PB6 / SDA1-->PB7 RCC->APB2ENR |= RCC_APB2ENR_IOPBEN; ...

SIDRI.1 by Associate III
  • 967 Views
  • 0 replies
  • 0 kudos

IS it possible to buid an applications that moves a circle around the screen on a STM32F42I discovery utilizing the BSP_LCD drivers? I've tried by deleting and drawing the new circle, but there is some flickering when I draw below 500 msec. Thanks, Piero

Here is the code. I'm looking for a solution that works with BSP_LCD (perhaps with other call)while(1){ HAL_Delay(300); x+=10; BSP_LCD_SetTextColor(LCD_COLOR_WHITE); BSP_LCD_FillCircle(BSP_LCD_GetXSize()/3+x-10, BSP_LCD_GetYSize()/3, CIRCLE_RADIU...

lvds / rgb connection tutorial

Hi I am new to embedded programming. I am currently using stm32f4 discovery board. I currently want to attach a lcd touch screen with my board. I have gone through some basic protocols fot displaying on lcd i.e via spi and i2c. I currently bought a 1...

MChau.11 by Associate
  • 1910 Views
  • 3 replies
  • 0 kudos

Problem about TouchGFX and I2C

Hi to all!I trying to run my first application of TouchGFX on custom hardware and I have some difficulties to integrate my code with the TouchGFX.At the moments. i can't use my I2C touchscreen driver. I have tested it in a test project and in this pr...

Luca1 by Senior
  • 1992 Views
  • 4 replies
  • 0 kudos