User Activity

I'm trying to use a KSZ8863 Ethernet PHY with the STM32F746G. We have used the RMII interface to connect with KSZ8863 and running at 50MHz frequency .RMII pins are connected to KSZ8863 based on MAC mode interface.To test the KSZ8863 ,We have used stm...
HiI have been using stm32F7 discovery board for USB Host interface.And I have created the TouchGfx project using Cube Mx .AndMy project is running on FREE RTOS. I have used the discovey USB host example .When connected the Pen-drive on USB-FS port, H...
HiWe have used touchgfx design in our customized STM32F746G project and using same hardware design of STM32F746G discovery board.While running, some wavy pattern is appearing on screen.I have attached the video for your reference .We have used FREE ...
While running of resistive display,some oscillations on the texts appeared on the screenSometimes noise came on display.I have attached the video that shows the display noiseCapacitive touch parameters(Vsync,Hsync) have been used for Resistive touc...
HiWe are trying to develop the custom external loader for our custom STM32F746Ng-MT25QT256 QSPI flash IC Before that we are trying to modify the external loader example project in ST utility for STM32F746G-discovery board,And we have created the N2...
Kudos from