STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! is Touchgfx unicode class UFT-16-LE or UTF16-BE?

Hello,I am trying to use FATFS file system from CubeMX. It ask me character encoding. There are some options "UTF-8", "UTF-16-LE" and "UTF-16-BE". I want to set it compatible with touchgfx unicode class. My question is which one is the touchgfx unico...

MuratUnal by Associate II
  • 1928 Views
  • 2 replies
  • 0 kudos

Resolved! Display problem when changing text of a textArea

Hello,Hello,I'm currently developing an application on a STM32H753VT6 with touchGFX and I have an issue with the function resizeToCurrentTextWithAlignment(). Indeed when i'm changing the current text (I use a Wildcard) with another text smaller there...

0693W0000059ihbQAA.jpg
AJT141 by Associate III
  • 3426 Views
  • 5 replies
  • 0 kudos

Issue with Touchgfx + stm32f769NI MIPI-DSI interface

Hi STM, we are working with MIPI DSI interface using STM32F769NI controller and 240x320 display resolution. We are having order of 10K if project is success.Firstly I have generated code using TouchGFX 4.14 and Immediately i have opened STMcubeMx 5.6...

kD1 by Associate II
  • 1603 Views
  • 2 replies
  • 0 kudos

Resolved! Possibility to use a data base

Hi everyone!The TouchGFX environment seems to be a powerful UI SW but I was wondering if it is possible to display values stored in a text (or other extention) file which is updated by Wi-Fi for example and stored into the memory. This so called data...

CClém.2 by Associate
  • 982 Views
  • 2 replies
  • 0 kudos

STM32H7B3I-DK LCD doesn't work well

Hello,I bought a STM32H7B3I-DK from https://www.mouser.com/. The new board had a demo project which using LCD to show different functions after opening box. However, when I downloaded the STM32H7 MCU package from st.com, compiled the ClockandWeather...

0693W00000594BGQAY.jpg
SDawn.1 by Associate II
  • 2125 Views
  • 3 replies
  • 0 kudos

DISPLAY PROGRAMMING CODE AND READ WRITE PROGRAMMING

Hi Team I am using STM32H7B31-DKI want to use display that is on the board and show my print messages on the screen I see that i want an application code that helps me to send the print messages data to the LCD on the board i see that there is nothin...

DRAME.1 by Associate II
  • 2595 Views
  • 8 replies
  • 0 kudos