cancel
Showing results for 
Search instead for 
Did you mean: 

MAX7219, 8-digit 7 segment LED display SPI programming

BGURR.1
Associate II

Could some one help me in making SPI C-program of MAX7219, 8 digit 7 segment display using STM32F401RE

 .

i have written this code in arm keil (µVision 5) it is not working, could someone help me please:

#include"stm32f4xx.h"

#include<stdio.h>

#include<string.h>

void Led_write (char data);

void delayMs(int n);

int main (void)

{

char num[] = {0x7e,0x60,0x6d,0x78,0x33,0x5b,0x5f,0x70,0x7f,0x7b};

RCC->AHB1ENR |= 0x0001;

RCC->AHB2ENR |= 0x1000;

GPIOA->MODER &= ~0xcf00;

GPIOA->MODER |= 0x8900;

GPIOA->AFR[0] &= ~0xf0f00000;

GPIOA->AFR[0] |= 0x50500000;

SPI1->CR1 = 0x031c;

SPI1->CR2 = 0x00;

SPI1->CR1 |= 0x40;

while(1)

{

for(int i=0;i<10;i++)

{

Led_write(num[i]);

delayMs(100);

}

}

}

void Led_write (char data)

{

while(!(SPI1->SR & 2));

GPIOA->BSRR = 0x00100000;

SPI1->DR = 0x0900 | data;

while(SPI1->SR & 0x80);

GPIOA->BSRR = 0x00000010;

}

void delayMs(int n)

{

for (int i=0;i<n;i++)

for (int j=0;j<3195;i++);

}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

You need to enable SPI clock in RCC.

It's probably better to use the symbols defined in the device header, rather than numbers, for the various register bitfields values.

JW

BGURR.1
Associate II

hello,

I have enable the SPI1 clock in RCC using RCC->AHB2ENR |= 0x1000; using this statement.

and i have tried new code, Please help me.

/* Micro controller: STM32F401RE

PA7  DIN

  PA5  SCK

  PA4  SS   

driver MAX7219: 8 digit 7 segment display */

#include"stm32f4xx.h"

#include<stdio.h>

void init_SPI1 (void);        // initialization of SPI1

void write_SPI1 (uint16_t data);   // writing data to SPI1

void delayMs (uint16_t n);      // generating delay

uint16_t shut_Addr = 0x0c00;  //Normal operation

uint16_t norm_Addr = 0x0c01;  //Normal operation 

uint16_t intn_Addr = 0x0a05;  //intensity register

//uint16_t code_Addr = 0x0900;  //address of decode mode

uint16_t dig1_Addr = 0x0100;  //selecting digit 1

int main (void)

{

init_SPI1();

write_SPI1(norm_Addr);

write_SPI1(intn_Addr);  // for intensity: intensity is 0x0e

while(1)

{

write_SPI1 (dig1_Addr | 0x01);  // for DIGIT1: sending value 3

}

}

void write_SPI1 (uint16_t data)  //writing something to MAX7219

{

while(!(SPI1->SR & 0x02));   //wait until transfer buffer empty

GPIOA->BSRR = 0x00100000;   //Slave select = 0

SPI1->DR = data;

while(SPI1->SR & 0x80);    //wait for transmission done

GPIOA->BSRR = 0x00000010;   //Slave select = 1

}

void init_SPI1(void)   //initializing the MAX7219

{

RCC->AHB1ENR |= 0x0001;  //Enabling clock of GPIOA

RCC->APB2ENR |= 0x1000;  //Enabling clock of SPI1

GPIOA->MODER &= ~0xcf00;  //resetting PA5, PA7: Alternate function and PA4: output function

GPIOA->MODER |= 0x8900;  //set PA5, PA7: Alternate function and PA4: output function

GPIOA->AFR[0] &= ~0xf0f00000;  

GPIOA->AFR[0] |= 0x50500000;  //set PA5, PA7: Alternate function

SPI1->CR1 = 0x0b14;      //seting baudrate, 16 bit format

SPI1->CR2 = 0x0000;

SPI1->CR1 |= 0x0040;      //Enabling SPI1

}

void delayMs(uint16_t n)     //generting of delay in n ms

{

for (int i=0; i<n; i++)

for (int j=0; j<3195; i++);

}

BGURR.1
Associate II

Following code is attached for reference