User Activity

Hello,In the documentation STM32 MC Motor Pilot :« Viewing and plotting registers with low-speed plotting.With this method of plot, any register can be plot but at low rate (polling every 200 ms by default) »I want to use the Motor Pilot plot (low sp...
Subject: position control of a brushless motor with encoder and FOC.I use a B-G431B-ESC1 to do position control on a brushless motor with an encoder and FOC. I want to make a trajectory from 0 to 276 rad in 0.833s. But currently, I can't make this tr...
Hi,I don't understand the calculation for Auto Calculate Torque/Flux Kp & Ki in Motor Control WorkBench (Version: 6.0.0)Could you send me the calculation formula because I can't find the same results. (I looked in your different documents and I can't...
Hello, I'm working with the STM32H7B3I-DK.Info:1- STM32H7B3I-DK (STM32H7B3LIH6QU)2-STM32CUBEIDE rev: 1.6.13- TouchGfx rev: 4.16.1I want to use the CRC module for data verification (16 bit).Problem:when I use the CRC default version everything works f...
Hello, I'm working with the STM32H7B3I-DK.I want to use this project in Romless and Xip (executable on OctoSPi).I just change the file .id (attached) , main.c (without MPU_Config()) and VECT_TAB_OSPI configuration. Problem:The pictures are not good (...