STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

I am missing a lot of the TouchCFX files after generating code with STM32CubeMX and "TouchCFX Designer". The linker errors is shown in the "Details". Should the code have been generated by "TouchCFX Designer" or have I missed something ?

Application/User/TouchGFX/target/TouchGFXHAL.o: In function `touchgfx::HAL::~HAL()':C:/workspace/test/test/CM7/Middlewares/ST/touchgfx/framework/include/touchgfx/hal/HAL.hpp:101: undefined reference to `vtable for touchgfx::HAL'Application/User/Touch...

FJahn.1 by Associate II
  • 2336 Views
  • 4 replies
  • 0 kudos

Resolved! The shape widget setAngle

When the shape widget is set to a new angle, it can not completely remove the disability from the previous angle. Is there a Bug or is there another way to solve this problem? Thank you!

0693W000006EkexQAC.png 0693W000006EkesQAC.png 0693W000006EkenQAC.png

Marquee text character from left to write

I have big text which I need to scroll left to right in loop with touch gfx. When I read more on it and found about scrollableContainer but kinda unsure how to combine it with my text object widget.I added below code   scrollableTripAdviceParameterTe...