STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Touchgfx color inversion

We are working on the TouchGFX with STM32H7 controller , able to display the images but colors are getting inverted on the LCD. TouchGFX and LTDC configuration looks fine. So what may be the issue.For Black <--> White Blue <--> Yellow Re...

KM L.1 by Associate II
  • 2121 Views
  • 3 replies
  • 0 kudos

Displaying analog voltage value on TouchGFX GUI using STM32F746G-DISCO kit. Display ADC value on LCD screen using TouchGFX.

https://www.youtube.com/watch?v=EbWOv_0Lp-U&t=1873sI saw this YouTube and tried to do the same.The textArea1Buffer variable declaration error occurred in Screen1View.cpp, and the screen was declared in Screen1View.hpp to complete the compilation.#inc...

Kss.1 by Associate II
  • 2879 Views
  • 3 replies
  • 1 kudos

Resolved! H750 PartialFrameBuffer

I use H750VBT6 FMC driver 800 * 480 LCD, due to internal SRAM is less than 800 * 480 * 2, so use PartialFrameBufferManager method.Because there is no TE pin in my LCD module.So I selected disabled when Cubemx generated the Partial Framebuffer VSync o...

lxw by Senior
  • 3763 Views
  • 6 replies
  • 0 kudos

How can I enable the DMA2D to have TouchGFX framework using it underneath the hood instead of using the CPU ???

I am using STM32H747I-DISCO and trying to enable DMA2D so that TouchGFX framework uses it for rendering and displaying images on the LCD instead of using the CPU.TouchGFX Designer 4.15.0 does not generate project files for my board (It supports lots ...

0693W000006I7mMQAS.png 0693W000006I7mWQAS.png
AGama.1 by Associate II
  • 1377 Views
  • 0 replies
  • 0 kudos

fastest method of drawing one pixel

Hello! I have a good 3d library https://github.com/FabioRM/dsp3D The author of the library ran it on STM32F746 . The library has the functionvoid dsp3D_LL_drawPoint(uint32_t x, uint32_t y, color32_t color) { if(x < minX) minX = x; if(x > maxX) ...

EEuge by Senior
  • 1617 Views
  • 5 replies
  • 0 kudos

Highlight a character within a text

I would like to highlight a single character within the text of a flex button. In my application I have an encoder with a button, which can change the numerical value displayed in certain increments, and I would like to switch the position of the hig...

AWies.1 by Associate III
  • 3987 Views
  • 9 replies
  • 0 kudos

Noob question. I have STM32H7B3I-DK and need to connect and grab info from the internet. Need a sample project.

So I'm new to this development.  I have STM32H7B3I-DK and need to connect to wifi/Internet and grab some data. I've experimented with TouchGFX Designer and there are templates that I like, especially the lens widget. Here are my questions:Is there...

TCygan by Associate II
  • 995 Views
  • 1 replies
  • 1 kudos

Resolved! AnalogClock and handleTickEvent()

Hi all,I would like to know how to use "handleTickEvent" on AnalogClock.I draw a screen with a Analog but thisone never upate itself.I see other examples witch use handleTickEvent to execute a new render but all has the same configurations..The stra...

MPast.1 by Senior II
  • 1516 Views
  • 4 replies
  • 0 kudos