STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! hex files

Thank you for helping.Environment: TouchGFX Ver 4.15.0What are the intflash.hex and target.hex files built and created by TouchGFX used for?Thank you.

Ebun.1 by Senior
  • 1484 Views
  • 2 replies
  • 0 kudos

Problems after updating to CubeMX 6.1 and Touchgfx 4.16

Hello,I have recently decided to try upgrading a project I have originally generated using CubeMx 5.6 and designed using TouchGFX 4.13 to CubeMx 6.1 and TouchGFX 4.16. After some teething problems, I have managed to get it working and running on my c...

SKILA by Associate II
  • 1800 Views
  • 3 replies
  • 0 kudos

Some confusion with the function names

HelloFirst of all, thanks for developing such a powerful tool and delivering us such a content rich documentation.I am playing with the partial framebuffer strategy, and I notice that, when the code is generated by the CubeMX, in the files TouchGFXHA...

PKriv.1 by Associate III
  • 2710 Views
  • 6 replies
  • 1 kudos

DSI howto check if command is send without error

uint8_t lcdRegData[2]; extern DSI_HandleTypeDef hdsi; void Wrt_Reg_3052(uint8_t Par1,uint8_t Par2) { lcdRegData[0]=Par2; HAL_DSI_LongWrite(&hdsi, 0, DSI_DCS_LONG_PKT_WRITE, 1, Par1, lcdRegData); } uint8_t NV3051D_Init(uint32_t ColorCoding,...

MM..1 by Chief III
  • 990 Views
  • 0 replies
  • 0 kudos

Where should we call the Screen1View::analogUpdate() function in the said video uploaded on Youtube.?

Hey,I am using STM32f429VIT6 and TouchGFX graphics library on my custom board I am not using any OS.I have refered to the video shared in the youtube @ the below location:https://www.youtube.com/watch?v=EbWOv_0Lp-Uwhere I am able to get the steady di...

STM32F767 LTDC + DMA2D + SDMMC = flickering

Hello! I have working system with LTDC + DMA2D run 800x600 at 32 MHz LTDC clock. In parallel there is configured SDMMC interrupt mode (no DMA) on 48 MHz and FatFs on it. And everything works fine. No glitches, no flickerings.Now I need to use 1024x7...

Resolved! Colors in LCD is lighter than TouchGFX design

recently, I am working on a project with STM32F746 and 9" LCD with GT911 touch panel, everything is working fine except the colors in the LCD appears lighter than expected in TouchGFX design! maybe something wrong with the settings So I uploaded some...

0693W000006G0E4QAK.jpg 0693W000006G03qQAC.png 0693W000006G0ArQAK.png 0693W000006G0EYQA0.png