STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

TouchGFX stop in takeFrameBufferSemaphore()

Still can't start works with #TouchGFX​. Target: make that touchgfx called function TouchGFXGeneratedHAL::flushFrameBuffer(rect);What I did:Start new project and select my chip (stm32f767z)switch on crcswitch on dma2d, and define color model rgb565, ...

0693W000008GNxFQAW.jpg

Resolved! Correct way to reload View?

I need to reload view completely after major external changes. I don't want to reset each state manually.What is the correct way to do this? Is this the only way?void MyView::reloadView() { application().gotoMyScreenNoTransition(); }This works fi...

Tuoman by Senior II
  • 1684 Views
  • 3 replies
  • 0 kudos

Resolved! cube ide ltdc touch gfx

I create a project on stm32f429zi nucleo, add LTDC, Touch GFX, CRC. I configure everything, add a BOX and a button. There are 3 errors when compiling. I tried it on different versions of CubeIDE and TouchGFX and different controllers. The only thing ...

Custom keyboard

hi team,Shown below images then you will get known my problemhow to adjust keywords to the keyboards

0693W000008GdqoQAC.jpg
HR M.1 by Associate II
  • 1788 Views
  • 3 replies
  • 0 kudos