STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Where can I find the source code of touchgfx library?

When I want to understand how touchgfx platform works, especially the operation on the framebuffer, I realize there are some functions I could not get the source code e.g. the functions swapFrameBuffers() and tick() below which seems to be defined in...

BParh.1 by Senior III
  • 3264 Views
  • 7 replies
  • 0 kudos

Resolved! STM32Cubemx configure FMC Nor Flash

When I use stm32cubemx to configure FMC Nor Flash, I can only configure Timing with Address setup time in HCLK clock cycles/Data setup time in HCLK clock cycles and Bus turn around time in HCLK clock cycles, but I think it should have more settings ...

0693W00000AO4aaQAD.bmp

Resolved! Where can I get the Demo binary firmware for external NOR memory on the STM32756G EVAL board?

I found a zip file on the Evaluation board with STM32F756NG MCU ​web page name “STM32756G-EVAL compiled demo binary 1.0�?,downloaded and unzip it. But it just some media files such as audio vedio picture and music. It has nothing about compiled binar...

TT.3 by Associate II
  • 3320 Views
  • 5 replies
  • 1 kudos

Tickles Mode implementation with RTOS Task

We are using a Custom PCB with STM32L4R9ZI. We are using it for GUI with Low power capabilities. And we are using RTOS and TouchGFX in our project.Do you guys have any documents or example code to implement Tickless mode in RTOS using multiple Tasks....