STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32F746IGT , 7 inch display With TouchGFX issues?

Hai i have a STM32F746IGT Development board and (Waveshare) 7inch display(800x480).Using tools are following bellow;STM32CubeIDE 1.6.1TouchGFX 4.16.0STM32CubeMX 6.2.1while run the code it's go to Hard Fault ();after doing some change in LTDC start ...

GMano.1 by Associate II
  • 1174 Views
  • 2 replies
  • 0 kudos

How can I unbind callback?

Hi ST engineers,I make a time-display-container and bind callback from RTC wakeup irq.Set binding operation in time-display-container init function.Unbinding it in destructor function.But my unbinding operation does not work.When RTC wakeup irq is c...

0693W00000BbQbuQAF.jpg 0693W00000BbQbkQAF.jpg 0693W00000BbQbpQAF.jpg
Zbobo.1 by Associate III
  • 1356 Views
  • 1 replies
  • 0 kudos

Resolved! How to version TouchGFX generated assets on OSPI flash?

Hardware:MCU: STM32L4R9ZGJ6OSPI Flash (512 Mb): MT35XL512ABA1G12Software:STM32Cube_FW_L4_V1.14.0STM32CubeIDE 1.6.0TouchGFX 4.13.0Hello,I am working on over-the-air device firmware updates for the STM application code and GUI assets stored in a memory...

DerekR by Senior
  • 1306 Views
  • 1 replies
  • 0 kudos

Scroll Menu container with hardware keys

Hi there, i'm really new to touchgfx and stm32 ecosystem and working on a project with multiple screens, were all has to be controlled with hardware buttons, the polling function for the buttons it's already implemented in a separate task and working...

GB.1 by Associate
  • 1905 Views
  • 3 replies
  • 0 kudos