STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Colors are distorted after loading 4.18.0

Hello,I was using 4.17.0 and I load 4.18.0. but after compiling and loading project to my board colors are distorted. Some colors are converted to blue,pink, red. It seems color settings are same in Touchgfx designer.How can I solve this problem.

Epamuk by Associate III
  • 3259 Views
  • 3 replies
  • 0 kudos

STM32f107Vbt6 controller interfaced with 3.2 inch ILI9341 display by using ST emwin GUI .After the LCD_X_DisplayDriver() function ,the debugger entered into HardFault handler() while debugging.(SPI Interface).GUI_DispString("Hello World!") is not working

In GUI_Conf.c, allocated the memory size for GUI.And in LCD_Conf.c file, declared the size of display ,configured the flexcolor driver for ILI9341 controller.And aslo implemented the read and write function by using SPI. In order to resolve the Hard...

Kanna by Associate III
  • 1485 Views
  • 2 replies
  • 0 kudos

TouchGFX Designer not working at all

Hello, I'm trying to get TouchGFX Designer 4.18 running with my H747-DISCO, but the download to the target fails every time. Thats the console output:   ST-LINK SN : 0024001E3137511439383538       ST-LINK FW : V3J8M3       Board      : STM32H747I-DIS...

MLang.7 by Associate III
  • 2066 Views
  • 3 replies
  • 0 kudos

Is it okay for TouchGFX function model::tick() to share resources with ThreadX, even though ThreadX is not aware of model::ticks() existence? Can they use the same mutex?

In my configuration, the tick source for touchGFX is the LTDC vsync interrupt. This was the recommended configuration in STM32CubeMX. However, that means that ThreadX is doing its own thing while model::tick (e.g., TouchGFX) is also running. The Thre...

Touchgfx compatibility with CubeIDE

i am trying to use stmcube IDE (1.8.0), cubemx (6.3.0)and touchgfx (4.18.0) for STM32H743IITX controller but i am getting tons of errors one after the other. Now,My Question is : All of these are compatible with each other? is there any dependencies...

Asing.4 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos

../TouchGFX/generated/videos/src/keil/Videos.s:1: Error: bad instruction `generated by videoconvert. Please,do not edit!'

Hi,I've just updgraded from TouchGFX 4.17 to 4.18. I'm using STM32Cube IDE 1.6.0.After regenerating the project from TouchGFX 4.18, when I build there is an error:"../TouchGFX/generated/videos/src/keil/Videos.s:1: Error: bad instruction `generated by...

Resolved! TOUCHGFX ... Add char to textarea ... How to add a char to the end of the text displayed in a textarea.

I do void Screen1View::updateAsciiInView(char* CwChar){ // add to txtbuffer Unicode::strncpy(textAreaAsciiBuffer, CwChar, 1); textAreaAscii.invalidate();}and that works fine ...my char i s displayed in the first position.But i need to add it to the e...

hjh by Associate III
  • 2895 Views
  • 4 replies
  • 0 kudos