STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

10bit Camera interface with STM32F7508-DK

Hello,We are working on interface of OV6946 camera with STM32F7508 development kit. We need to capture image and stream on STM32F7508 Display. Camera which we are using provides 10bit output with 400x400 resolution in Bayer’s format. The connections...

NS.9 by Associate II
  • 5468 Views
  • 11 replies
  • 0 kudos

Is STM DCMI driver support Raw Bayer Image format?

I'm interfacing 10-bit camera on DCMI protocol. I can able to read the data over DCMI and display it on the STM32F7508 Discovery board. Since the color format is different I'm not getting the actual real-time colors. I'm using the "Camera" example on...

Rio1 by Associate
  • 1671 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX porting process

Hi,I was wondering what the TouchGFX porting process is like for development across different MCUs.I'm thinking of starting development for a GUI on an STM32 Discovery Board, and then when the actual hardware gets produced, switch over to developing ...

DOkaz.1 by Associate II
  • 2029 Views
  • 2 replies
  • 0 kudos

After update of Touch GFX, Colors on the display (Hardware) are not the same than on the simulator. | Alpha factor isn't working (Opacity)

After updating my project, from 4.15.0 to 4.18.1 the colors displayed on the display are not the same that those on the simulator.The simulator works fine colors are correct.Moreover I observed something strange:If I set the color depth at 16 bpp : C...