cancel
Showing results for 
Search instead for 
Did you mean: 

10bit Camera interface with STM32F7508-DK

NS.9
Associate II

Hello,

We are working on interface of OV6946 camera with STM32F7508 development kit. We need to capture image and stream on STM32F7508 Display. Camera which we are using provides 10bit output with 400x400 resolution in Bayer’s format.

The connections are done as mentioned below:

Camera Pin Controller Pins

DCMI_D0            -             PH9

DCMI_D1            -             PH10

DCMI_D2            -             PH11

DCMI_D3            -             PH12

DCMI_D4            -             PH14

DCMI_D5            -             PD3

DCMI_D6            -             PE5

DCMI_D7            -             PE6

DCMI_D8            -             PI1

DCMI_D9            -             PI2

DCMI_PIXCLK   -             PA6

DCMI_HSYNC   -             PA4

DCMI_VSYNC   -             PG9

DCMI_SDA         -             PB9

DCMI_SCL          -             PB8

We are using example code from STM32 Cube example project named “Camera�?.

We are getting black and white scrolling image for the configuration given below

static void LCD_LL_ConvertLineToARGB8888(void *pSrc, void *pDst)
{  
  /* Enable DMA2D clock */
  __HAL_RCC_DMA2D_CLK_ENABLE();
 
  /* Configure the DMA2D Mode, Color Mode and output offset */
  hdma2d_eval.Init.Mode         = DMA2D_M2M_PFC;
  hdma2d_eval.Init.ColorMode    = DMA2D_OUTPUT_ARGB8888;
  hdma2d_eval.Init.OutputOffset = 0;
 
  /* Foreground Configuration */
  hdma2d_eval.LayerCfg[1].AlphaMode = DMA2D_NO_MODIF_ALPHA;
  hdma2d_eval.LayerCfg[1].InputAlpha = 0x00;
  hdma2d_eval.LayerCfg[1].InputColorMode = DMA2D_INPUT_RGB888;
  hdma2d_eval.LayerCfg[1].InputOffset = 0;
 
  hdma2d_eval.Instance = DMA2D;
  
  /* DMA2D Initialization */
  if(HAL_DMA2D_Init(&hdma2d_eval) == HAL_OK)
  {
    if(HAL_DMA2D_ConfigLayer(&hdma2d_eval, 1) == HAL_OK)
    {
      if (HAL_DMA2D_Start(&hdma2d_eval, (uint32_t)pSrc, (uint32_t)pDst, 200, 1) == HAL_OK)
      {
        /* Polling For DMA transfer */
        HAL_DMA2D_PollForTransfer(&hdma2d_eval, 100);
      }
    }
  }
  else
  {
    /* FatFs Initialization Error */
    while(1);
  }
}

Please refer the link below for output reference:

https://drive.google.com/file/d/1ATyK06csLdJNzLO_H6x2dtP0buMR2cGr/view?usp=sharing

Please guide us, what are the built in configurations are need to be used for converting 10bit Bayer image input to RGB LCD output.

Thanks & Regards,

Ayaz Ahmed,

Riosh Technologies,

Bangalore.

11 REPLIES 11
KDJEM.1
ST Employee

Hi @NS.9​ ,

The “Application note Digital camera interface (DCMI) for STM32 MCUs�? (AN5020), mentioned an example with RGB data capture.

I advise you to refer to this application note to resolve the problem.

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

NS.9
Associate II

The camera output is in raw Bayer format like below

0693W00000NrqIKQAZ.pngHow do we convert this to RGB format. We had referred the same document, can you please point out in the document where we can refer RAW data to RGB conversion.

NS.9
Associate II

We have successfully able to print color image on the display. But the Video streaming is scrolling vertically slowly.

Can you please share your view on this, what might be the cause for scrolling.

KDJEM.1
ST Employee

Hi @NS.9​ ,

Glad to know that initial issue is already fixed.

Regarding the new issue: could you please share the code that can help to reproduce it so that I can investigate on my side?

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

NS.9
Associate II

.

NS.9
Associate II

.

NS.9
Associate II

From the example code 'CAMERA' for STM32F7508-DK.

main.c/ "static void LCD_LL_ConvertLineToARGB8888(void *pSrc, void *pDst)" function we have configured DMA2D_Input_Color_Mode macro to DMA2D_INPUT_RGB888 and we are getting color image but the colors are not identical, in the place of yellow color we ara getting blue color and in the place of blue we are getting yellow color. This may be because of Bayer's color format. We tried all the macros mentioned below under DMA2D_Input_Color_Mode.

DMA2D_INPUT_ARGB8888    0x00000000U 

DMA2D_INPUT_RGB888      0x00000001U 

DMA2D_INPUT_RGB565      0x00000002U

DMA2D_INPUT_ARGB1555    0x00000003U

DMA2D_INPUT_ARGB4444    0x00000004U 

DMA2D_INPUT_L8        0x00000005U 

DMA2D_INPUT_AL44       0x00000006U 

DMA2D_INPUT_AL88       0x00000007U 

DMA2D_INPUT_L4        0x00000008U 

DMA2D_INPUT_A8        0x00000009U 

DMA2D_INPUT_A4        0x0000000AU 

Can you please share the configuration for Bayer format.

@NS.9​ has also started a separate thread on this:

https://community.st.com/s/question/0D53W00001eYOHJSA4/conversion-from-raw-bayer-format-to-rgb-format-in-stm32f7508dk

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

It looks like there isn't real support for RAW Bayer in the DMA2D_Input_Color_Mode, as far as I can see. That's surprising, because the AN5020 clearly says it does. Maybe the hardware is capable but the code hasn't been written yet.

Can anyone confirm this?

Alternatively, you could of course use an older camera module with DVP (parallel) and RGB565 output support.

Thanks