STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

sd card not working with touchgfx

Hi, I tried the example on formatting the sdcard and it works (https://www.youtube.com/watch?v=I9KDN1o6924).How do I implement this with TouchGFX? I set everything the same and mount the SD card (f_mount), but the next command is no longer executed (...

JNova.0 by Associate III
  • 1787 Views
  • 4 replies
  • 0 kudos

Resolved! Widget move across container.

Hi, I used a swipe container with 2 pages, and I want to drag the icon from the 1st page to the 2nd page. But the icon cannot move to 2nd page because the icon is create in the 1st page container and doesn't move across container. How can achieve m...

V.H by Senior
  • 1184 Views
  • 1 replies
  • 0 kudos

Resolved! Simulator - Using key presses as inputs?

Hello,I noticed there is a way to print to a console from the simulator using touchgfx_printf, I'm wondering if it's possible to read in characters also?I noticed the comment in Utils.hpp:The console window is used to print to using touchgfx_printf()...

AMars.4 by Associate III
  • 3856 Views
  • 5 replies
  • 0 kudos

Resolved! How to modify STM32Cube Project in TouchGFX

Hey,i use the STM32H757-EVAL Board and was already able to create a new project in TouchGFX (4.20.0), import it to STM32CubeIDE (1.10.1) and modify GUI and Hardware functionality.In order to have more flexibility and to setup a more clean project, i ...

JMuller by Associate II
  • 3702 Views
  • 4 replies
  • 0 kudos

beginFrame and endFrame is locked after a while

Hello, I have a project with STM32L4R9AI and touchgfx. I use DSI for amoled display. I am developing codes for months. At some point screen is started to be locked ( no changes in screen ). While debugging the code when I look at the freeRtos task ta...

Epamuk by Associate III
  • 2777 Views
  • 4 replies
  • 0 kudos

Resolved! LCD replacement for STM32F429I-DISC1

Hello,I have borrowed an STM32F429I-DISC1 with 2.4" QVGA TFT LCD.Unfortunately, I fumbled it and cracked the screen.I'd like to fix it for my friend, but don't want to start tinkering if it'll cause a problem.Does anyone have experience in replacing ...

Dwait.1 by Associate II
  • 3487 Views
  • 6 replies
  • 0 kudos