STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Issue: Widget overwritten.

Hi, For example, I create 2 widgets (button and box), the box in top and button in bottom.I need to change their position like picture 2, how can I do except delete and rebuild to changed their order ?  

0693W00000QNRVaQAP.png 0693W00000QNRVkQAP.png
V.H by Senior
  • 1077 Views
  • 3 replies
  • 0 kudos

Resolved! Tutorial 2: Call New Virtual Function Overwriting Code

I am new to TouchGFX and STM32 programming, so I apologize if any obvious details are missed. I am attempting to run Tutorial 2 in the TouchGFX tutorial (Because I'm a new member, I cannot add the link, but it's the TouchGFX Version 4 19 tutorial gui...

KMew by Senior III
  • 1581 Views
  • 4 replies
  • 0 kudos

Where should my DCMI buffer point to?

Hi,I am trying to interface an OV7670 camera module with the F746 NUCLEO board and was wondering if the f746 chip's DMA has only a specific memory area where it works.The image resolution will be QCIF so buffer has to be 50688 byte long.thanks

MRoso.1 by Associate II
  • 1531 Views
  • 2 replies
  • 0 kudos