STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

ST emwin library issue

We are using the emWIN library to display the images, but we are having problems. The initial screens 2 are displaying, but when you enter a specific screen, the display module does not respond.We can't figure out what's wrong because it's structing ...

MRedd.3 by Associate II
  • 1738 Views
  • 2 replies
  • 0 kudos

Does the STM32F have separate video memory?

I am currently looking for a microcontroller or processor with MIPI DSI output. The STM32 devices have this, but there is something that does not seem to make sense. They only have 512kB of internal memory. This would not be enough to hold a single f...

HElia.1 by Associate II
  • 2513 Views
  • 4 replies
  • 0 kudos

Resolved! Stemwin update plan

Hi, are there any future plans on updating emwin base in stemwin lib ? If I didn't miss something latest update was V5.44 / 22-March-2018.

JureL by Senior
  • 3143 Views
  • 6 replies
  • 0 kudos

TouchGFX: Query for technical details

We are evaluating TouchGFX and its performance in details. Can anyone please provide some technical details regarding below criteria, that would be appreciated.UI reusability(means is it possible to modified the UI assets of already created UI)Graphi...

maulesh by Associate II
  • 2007 Views
  • 4 replies
  • 0 kudos

STM32H747- Disco, CubeIDE v.1.10.1 Error during the following: Hi All, I'm having trouble to determine the reason why even a basic screen (white bckgrnd with 3-10 text letters) fail to display CM7. This happen with SD Card peripheral with CM4.

Memory stack/heap size were increased. Even tried to use DMA with no change.The screen is dimmed and colors aren't the ones designed. I'm learning about the DMA setup for this Kit so, knowledge about it's complete setup is unknown to me.Also, when tr...

Resolved! How to configure TOUCHGFX on the custom board in bare metal & without the use of external memories.

Hi...I am using STM32H750I Board with resolution of 480 x 272 , but I have a to configure board with 480 x 480 resolution. How can I customize the board in TOUCHGFX IDE in bare metal?Can I use only Internal memory to store the framebuffer, not extern...

PM.5 by Associate III
  • 1612 Views
  • 2 replies
  • 0 kudos