STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Bug with Graph / Histogram

Hello,Coudn't find a Bugtracker, so I posted it here.I use a static graph in my project, but after some time (adding other stuff) the TouchGFX-Designer (4.20) creates incomplete code:This happend several times, only fix is to remove and add a new dia...

0693W00000WIVwyQAH.png 0693W00000WIVxSQAX.png 0693W00000WIVzOQAX.png
PBull by Associate III
  • 2678 Views
  • 4 replies
  • 0 kudos

Resolved! H743I Eval2 board is working with TouchGFX to display data. but unable to activate ETH and lwip middleware with CubeIDE.

I use H743I Eval2 board , able to build application with TouchGFX to display data. I am trying to activate ETH with lwip middleware with CubeIDE. have enable CORTEX_M7 (Icache,Dcache) but can not select any mode (MII, RMII) in ETH, (a forbidden mark ...

ET.2 by Associate III
  • 3874 Views
  • 6 replies
  • 0 kudos

Resolved! initially, touchgfx + cubeide is OK, but when changing setting from ioc , will casue some error: no declaration matches ...

I uses touchGFX associated with Cube IDE with ETH, lwip freertos , it is compiling ok and working. But found ETH gpio pin of ETH in ioc, the max speed is setting to low, so I change it to veryhigh , rebuid the code found a new TouchGFX folder is cre...

0693W00000aJIH2QAO.png 0693W00000aJI0KQAW.png 0693W00000aJI1kQAG.png 0693W00000aJIIUQA4.png
ET.2 by Associate III
  • 2609 Views
  • 3 replies
  • 0 kudos

Resolved! STM32 LTDC Simple Text String Output to LCD

I have successfully setup the LTDC to work with my LCD to display TouchGFX images with no problems. However, I am also developing a simple bootloader for USB software updates that I need to display text to the display without the use of RTOS or Touc...

PFlor.2 by Senior II
  • 4919 Views
  • 5 replies
  • 0 kudos